STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F1 USB in CDC mode

Posted on August 19, 2016 at 10:38 Hello there, I am struggling with this issue for over a (whole) day now... I have a custom STM32F103VBT6 board. I am trying to power up USB in CDC mode. I am using CubeMX to generate the code. At first, my ...

where i can find an example for dual CDC VCP on stm32?

Posted on August 17, 2016 at 00:56I should use the USB FS on CN5 of STM32F4-Discovery in dual Virtual Com Port (if possible in three VCP).I made a project started from cubemx with USB_CDC_VCP with USBD_MAX_NUM_INTERFACES = 3 and USBD_MAX_NUM_CONFIGU...

mirko2399 by Associate II
  • 1714 Views
  • 3 replies
  • 0 kudos

SPI Timeout problem

Posted on February 28, 2016 at 16:15Hi,I'm using ST's driver for SPI in full -duplex, 8 bit, master mode. The function HAL_SPI_TransmitReceive() returns sometimes HAL_TIMEOUT. After inspecting code I don't understand the following:The code below at ...

ari_v2 by Senior
  • 4207 Views
  • 4 replies
  • 0 kudos

[STM32L4] [USARTx] How to configure USART as a wakeup source

Posted on August 08, 2016 at 06:14Hi,I am using USART interface - Rx as Interrupt and am configuring the Rx as 1-byte receive interrupts.Is there a way by which, this interface can be configured explicitly as a wake-up source like we get the interru...

sunny by Associate II
  • 1818 Views
  • 2 replies
  • 0 kudos

Where to find X-CUBE-AUDIO-F7 firmware ?

Posted on August 17, 2016 at 13:33Hello, I didn't found on the ST web site the libraries pointed by https://www.google.fr/url?sa=t&rct=j&q=&esrc=s&source=web&cd=4&cad=rja&uact=8&ved=0ahUKEwjRgs3AkqvOAhXQzRoKHSnEBBcQFgg0MAM&url=http://www.st.com/reso...

jmf1 by Senior
  • 1140 Views
  • 2 replies
  • 0 kudos

About HAL_UART_Receive_IT arguments

Posted on August 18, 2016 at 18:33 One slip of my finger and my post was gone. I hope this is not a duplicate post. I am receiving serial data one byte at a time. For that I need an one byte array, I think. Does it have to be an array? O...

LMI2 by Lead
  • 1162 Views
  • 1 replies
  • 0 kudos

Key matrix example code

Posted on August 18, 2016 at 17:52Hello,I need 4x4 key matrix IAR example C source code for STM32F series.It would be very helpful for me if you can give me.Thanks in advance! #key-matrix #keypcad

w21685 by Associate II
  • 1334 Views
  • 1 replies
  • 0 kudos

SDRAM connections on FMC

Posted on August 18, 2016 at 17:55Hi,Hoping for some feedback from ST or others who have tested/used this configuration...The datasheet for the STM32F745xx (also the 746xx) contains Table 11. This shows the FMC pin definition, and lists the followin...

STM32F405 corrupt i2c transactions

Posted on August 17, 2016 at 14:06Hi!I have been writing my own I2C driver to play well with the RTOS and I have been using a I2C analyser to help me out. After a lot of frustration I have gotten most of it working but what I have discovered is that...

0690X00000603BHQAY.jpg
tobias by Associate II
  • 1844 Views
  • 2 replies
  • 0 kudos