Question
Problem reading SD card
Posted on March 11, 2016 at 20:08
Hi to all,
I have a big issue with SD cards. I initialize correctly my sd card, but when I try to read a block, I can read it only the first time. This is my routine: ===================== uint32_t MYSD::ReadSector(uint32_t sector, uint8_t *block) { uint8_t t; uint16_t i; GPIOA->BRR = 0x01<<SDSS0; // Set SDSS0 low t = CommandAndResponse(SPICMD17, sector); //Read sector command if(t != 0) { GPIOA->BSRR = 0x01<<SDSS0; // Set SDSS0 high myusart1.PrintString((uint8_t *) ''Cannot read (CMD17)'', ' ', 0); myusart1.PrintHex8(t); myusart1.PrintChar('\n'); return 1; } do { t = sp->Transfer8(0xFF, 0, 0); // Wait for card response } while(t == 0xFF); if(t != 0xFE) { GPIOA->BSRR = 0x01<<SDSS0; // Set SDSS0 high myusart1.PrintString((uint8_t *) ''Cannot read (Token response)'', ' ', 0); myusart1.PrintHex8(t); myusart1.PrintChar('\n'); return 2; } for(i=0; i<512; i++) block[i] = sp->Transfer8(0xFF, 0, 0); //Read data t = sp->Transfer8(0xFF, 0, 1); // Read CRC t = sp->Transfer8(0xFF, 0, 1); // Read CRC GPIOA->BSRR = 0x01<<SDSS0; // Set SDSS0 high return 0; } ===================== and this is the tesponse: Iteration 1: CMD17 response 0 Iteration 2: CMD17 response 4 Iteration 3: CMD17 response 0 Iteration 4: CMD17 response 4 Iteration 5: CMD17 response 0 Iteration 6: CMD17 response 4 Iteration 7: CMD17 response 0 Why I can read block in odd iterations and not in even? The routine is always the same. Anyone encountered the same problem? Thank you Freya