STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103C6T6A clock configuration

Posted on September 27, 2016 at 17:30I need to configure the system clock to HSE with a 8MHz quartz crystal.At startup the default is HSI. For the STM32L family I used the clock configuration tool provided by ST, but this tool is not available for S...

Jump to user application in the USB_Device/DFU_Standalone Example

Posted on September 27, 2016 at 14:48Hello,I am using STM32Cube_FW_L4_V1.5.1 library and I am trying to test the STM32Cube_FW_L4_V1.5.0\Projects\STM32L476G_EVAL\Applications\USB_Device\DFU_Standalone application. I have STM32L476RG-Nucleo + NUCLEO-C...

dpn by Associate II
  • 1930 Views
  • 3 replies
  • 0 kudos

CAN is getting stuck in initilaztion

Posted on September 27, 2016 at 03:34Hi,I m using STM32F303XC processor.I configured the CAN at 250 kbps baud rate. but it is getting stuck in following while loop. CAN is not able initialize properly.What would be the problem to getting stuck in in...

SS.Sagar by Associate III
  • 1572 Views
  • 4 replies
  • 0 kudos

STM32F407 Dual DAC Independent Trigger Sources

Posted on September 27, 2016 at 08:54Hello,I have a problem for using both DACs of STM32F407 with independent trigger sources. What I did was directing DAC1 for Timer6 and DAC2 for Timer7 but they are still both triggered by one source (Timer6) and ...

yousef by Associate
  • 1346 Views
  • 2 replies
  • 0 kudos

Flush USART RDR after receiving

Posted on September 27, 2016 at 17:11Dear all,I am using STM32F4 Discovery board and have some problems with using DMA on USART. The cause may be the unwanted left behind data inside USART RDR.Would you please kindly give me instruction how can I fl...

Problem with debugging & IWDG with STM32F407VGT6

Posted on September 21, 2016 at 15:56Since firmware version 1.13 there is a big issue with debugging. The firmware starts the watchdog during initialization. This result in reset when a breakpoint reaches. Before this version, I could start the IWD...

Osto by Senior
  • 1165 Views
  • 2 replies
  • 0 kudos

STM32F411 Errata

Posted on September 24, 2016 at 16:20Is there a new version of the Errata document? The one the website (Doc ID 027036) is revision 1 and was released on 20-Oct-2014.Why do I ask? The STM32F412 - has an Errata about DMA2 corruption when managing AHB...