STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to connect ST CONTROLLER TO INTERNET

Posted on September 29, 2016 at 17:10Hello        Greeting to all!  I have STM3220G EVAL Kit. I am facing problem on Window 10 PC while using Echo Tool.it is not responding.Kindly suggest  the solution & reason behind the problem.I want to connect...

dushyant by Associate
  • 1021 Views
  • 1 replies
  • 0 kudos

STM32L073CZT - DfuSe Demo - Internal Flash Problem

Posted on September 21, 2016 at 15:04Hi,I have a Problem with a STM32L073CZT  on chip bootloader and the DfuSe Demo (v3.05).It is not possible to upload or down Load from/to the InternalFlash.Downloading or Uploading the DATA Memory is possible.Does...

0690X00000605RuQAI.png 0690X00000605JuQAI.png

SP1ML (SPIRIT1 and STM32L1)

Posted on September 27, 2016 at 17:07Hi,I've just got the steval-sp1ml868 and have been trying to gave it communicate with TI transceivers CC1111/CC1101. The TI transceiver works in the same 868 MHz and so far I have been able to receive radio messa...

sean23 by Associate II
  • 1304 Views
  • 2 replies
  • 0 kudos

Wrong entry point

Posted on September 27, 2016 at 12:47 Hello, I am using TrueStudio for STM My problem is, that when I start debugging the PC (program counter) shows an address of0xf3af48 As this address is somewhere in nomansland the Dissassembly shows ''...

machinist by Associate III
  • 1377 Views
  • 2 replies
  • 0 kudos

No interrupt from DMA

Posted on September 29, 2016 at 15:13 I'm trying to receive serial data using USART1 and DMA in 3 different chunks. Between I'm setting the buffer size in the DMA (2 bytes, 1 byte, 10 bytes) using the function set_ dma _buffer_...

heinz by Associate II
  • 1519 Views
  • 2 replies
  • 0 kudos

Prescaler Value for the Timer in Encoder mode

Posted on September 29, 2016 at 16:42I am using TIM4 of STM32F767 in Encoder mode. The period is set to 1000. The CNT value changes as follows: 0->1000->1->1000->0 and so on. On monitoring the DIR bit, I found that it keeps oscillating between 0 and...

Neo M by Associate II
  • 793 Views
  • 0 replies
  • 0 kudos

VCP driver issue for Windows 7. can recognize in Windows 10

Posted on September 16, 2016 at 23:29Hello all. Windows 10 can well recognize my STM32L1 device (custom PCB) as 'USB Serial device' but same isn't recognizing in Windows 7 (another PC). I've tried both VCP driver 1.3 and 1.4 in windows 7. Do I need ...

rumlyen by Associate II
  • 841 Views
  • 1 replies
  • 0 kudos

STM32F2 CAN Bus HAL Driver problem

Posted on September 29, 2016 at 12:29Hi This is my first post on this forum, so please excuse me if I don't follow the correct procedure. I think there are a problem with the STM32F2 HAL firmware driver version 1.4.0. I am using IAR Embedded workben...

pieter2 by Associate
  • 1516 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.