STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F205RG USART1 transfering not same string.

Posted on October 04, 2016 at 07:17Hello, everyone. AccessPort app was used for test. AccessPort prints ''0x00, 0x55, 0x55, 0x55, 0x55, 0x55, 0x79, 0x3D'' Test code is as follows; int main(void) {     char szTemp[8] = {0x55, 0x55, 0x55, 0x55, 0x55, ...

tony1987 by Associate
  • 761 Views
  • 2 replies
  • 0 kudos

STM32F030 and X-CUBE-WIFI1

Posted on October 03, 2016 at 21:22Hi all, I'm developing a solution with a STM32F030 and a serial-to-WiFi module SPWF01SA. I downloaded the expansion package X-CUBE-WIFI1 from ST website that provides sample implementations for others NUCLEO like a...

Problems setting up clocks, STM32F401RE

Posted on October 04, 2016 at 09:47Hello I am using a nucleoboard and am trying to set up all the clocks using this: RCC_ClocksTypeDef RCC_Clocks; RCC_HSICmd(ENABLE); RCC_HCLKConfig(RCC_SYSCLK_Div1); RCC_PCLK2Config(RCC_HCLK_Div1); RCC_PCLK1Config(R...

Bug on USB DEVICE EP0StartXfer ?

Posted on October 04, 2016 at 11:43Hi, I made a small project for USB device with STM32F415, but I have a problem. I receive setup data from the PC on EP0 , but when I write data (which should come out from Device to Host) these data not exit.Moving...

Marco1 by Associate II
  • 609 Views
  • 1 replies
  • 0 kudos

Which interrupt for complete uart transfer with DMA

Posted on September 13, 2016 at 15:07Hi, With STM32L1, I need to know when a frame transmition is complete when sent on uart using DMA. By complete, I mean, the last bit has been sent on the line because I need to activate a buffer when data is tran...

JulienD by Senior
  • 1422 Views
  • 4 replies
  • 0 kudos

USB Hub controller interfacing

Posted on October 04, 2016 at 12:03Hey Guys, please anyone help to interface STM32F429VGT6 with the usb hub controller of TI. Anybody is having the program to communicate with the  USB hub controller? Is it possible to communicate with the many USB ...

dixon by Associate II
  • 551 Views
  • 0 replies
  • 0 kudos

Select STM32 for 3-Phase PFC?

Posted on October 02, 2016 at 23:06Hello,I design 3 phase PFC controller in very high power rate up to 800kW with another manufacturer microcontrollers. But nowadays I want to jump ARM area. In this case, I choose STM32F334 micro and working its dis...

STM32F429 GCC stack size error with personal DFU

Posted on October 03, 2016 at 13:52Hi everyone!I'm GUI programing with STM32F429GI.I've two application which one is myself DFU app and other is Main Application.DFU is located flash at 0x8000000 to 0x800BFFFAnd Main application start 0X800C000.STM3...

echonoh by Associate
  • 1383 Views
  • 2 replies
  • 0 kudos

Extract code from STM32F4DISCOVERY

Posted on October 03, 2016 at 08:33Hi, Can some one help me how to extract my code from STM32F4DISCOVERY KIT? I lost my code in my PC. I'm using IAR Embedded Workbench platform to program my STM32F4DISCOVERY KIT.

Resolved! STM32L073: RTC Wakeup event not exiting STANDBY mode

Posted on September 22, 2016 at 20:33I have the development board for the STM32L073 and have been testing the functionality of the board regarding waking up from STANDBY mode. I have been able to get it to wakeup only use the IWTG funcitonality. I h...

conner by Associate II
  • 3253 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.