cancel
Showing results for 
Search instead for 
Did you mean: 

I2S Channel Side Flag Issue

officialkesh
Associate III
Posted on April 14, 2016 at 16:31

Hello ,

I have configured I2S3ext of STM32F4 which is interfaced with audio codec.

In our environment ,

Sample Frequency is  @ 8 KHz .

CHSIDE bit of I2S status register always remains in reset state .

I have checked no overrun flag has not been set .

What could be the other reason for not setting this CHSIDE bit ?

- Pinkesh

#i2s-channel-side-issue
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on April 14, 2016 at 17:27

> I have configured I2S3ext

Transmitter or receiver? Which mode? Post perhaps the I2S3ext registers' content.

Which pins are you using for I2S3/ext?

JW

officialkesh
Associate III
Posted on April 15, 2016 at 08:20

Hi Jan,

In our environment ,

PC11 - I2S3ext _SD line 

PC12 - I2S3_SD line

PC10 - I2S3_CK

PA15 - I2S3_WS  line

I2S3 as full duplex in which I2Sext configured as Slave receiver & I2S as Slave Transmitter while external device work as I2S master .

After configuring I2S,

SPI3 Peripheral contents are

CR2 - 0x80

SR - 0x02

I2SCFGR - 0xC00

I2S3ext Peripheral Contents are

CR2 - 0x40

SR - 0x02

I2SCFGR - 0xD00

- Pinkesh