STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CMSIS-RTX with GCC on STM32F4 Discovery

Posted on October 03, 2016 at 21:38I was successfully able to adapt CMSIS-RTX in a Discovery_F4 based project (MP3 Player) using Atollic TrueSTUDIO ARM v6.0.0 Lite version which is a free professional quality toolchain based on GCC and Eclipse. The...

rverma by Associate
  • 947 Views
  • 1 replies
  • 0 kudos

STM32L05xx HSI problem with VDD = 1.8v

Posted on October 10, 2016 at 14:08I have a STM32L051K8T6 which I am running from a 1.8v supply to interface with a Quectel UG95 modem.  Project produced with STM32CubeMX. Code is compiled with Keil uVision 5.21a. The firmware continually reboots ab...

Noise with DMA/ADC

Posted on September 30, 2016 at 06:33We are running a number of channels of ADC on the STM32F0-Discovery board. We have the code below configured to continually read the input signal levels.  The code is based on routines posted elsewhere in this fo...

0690X00000602QoQAI.bmp

STM32F103RBT6 complimentary output polarity problem

Posted on October 10, 2016 at 01:11Hi,I am trying to get complimentary output working with the same polarity on both the OCx and OCxN.  I have successfully done this with TIM_OCPolarity_High, and TIM_OCNPolarity_Low.  The next step is to be able to ...

STM32F103 resetting

Posted on October 10, 2016 at 09:35Hi, I have an STM32F103RC8 controller board. I have two LEDs connected to two port bits. When I load a using flash loader demo program to toggle the LEDs the program works for a few seconds and the controller reset...

nps by Associate II
  • 1255 Views
  • 1 replies
  • 0 kudos

Possible mistake in DMA channel 3 selection for STM32L0x2

Posted on October 08, 2016 at 16:31Found a possible mistake in ''DocID025941 Rev 3'' page 276 in C3S[3:0] description    1100: DMA channel 3 remapped to USART4_TX  1101: DMA channel 3 remapped to USART4_TX Is it real routing scheme or it should be ...

dmitrystu by Associate II
  • 1041 Views
  • 1 replies
  • 0 kudos

STM32F4 multi-channel input capture interrupt confusion

Posted on October 10, 2016 at 01:34 I was hoping to get some clarification on a topic that has me confused with the STM32F4. I'm wanting to use all four channels of Timer2 for measuring period and the number of events for four different incoming ...

mvaras101 by Associate II
  • 2334 Views
  • 1 replies
  • 0 kudos

STM32F4 discovery SPI issue

Posted on October 09, 2016 at 07:06Hello,         - I am using STM32F4 discovery board to send data via SPI. i have got it working but there is a small issue. the SS pin goes high before the the mcu finishes sending data. i am using SPI1, and used ...

0690X00000605c9QAA.png 0690X00000605cAQAQ.png