STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to tell if other CAN device is present on bus?

Posted on November 28, 2016 at 04:58I would like to know if there is another device present on the CAN bus.  Is there a way to do this without too much overhead?  I have my STM32F4 setup and communicating on a CAN bus.  Sometimes there is another de...

I2C Questions on STM32F427

Posted on November 25, 2016 at 09:35I have a slave device which is address 0x78 for write and address 0x79 for read.I want to confirm that why the below I2C transaction is difference?I want to reset the slave device and the mapping register informat...

0690X00000605SxQAI.png 0690X00000605SUQAY.png
pohua by Associate II
  • 1222 Views
  • 2 replies
  • 0 kudos

ST-Link V2 dongle broken?

Posted on November 26, 2016 at 11:20Purchased from Mouser 1.5 years ago but not used until now. I am getting ''Can not connect to target!'' error message in ST-Link Utility whether I try my Mini-M4 for STM32 (415RG, JTAG/SWD) or my Discovery board (...

parsec by Associate III
  • 2132 Views
  • 4 replies
  • 0 kudos

ST-Linkv2 Pod: Connection in ''Low Power Mode''

Posted on November 27, 2016 at 00:48Hi, Sorry if this question may have been answered, I was unable to find anything in the forum on this. Using an STM32F405/64pin device. Boot 0 is tied to GND through a 470R resistor. Since I'm using flash boot, I ...

Dubious update of TIM8_DMAR

Posted on November 26, 2016 at 15:52 When debugging an application I wondered about a strange value in TIM8_DMAR that I had not written there intentionally. In the end it all boiled down to an invocation of LL_TIM_SetCounterMode (TIM8, LL_...

Stm32f1cube bug on debug

Posted on November 22, 2016 at 09:37When i enable SWD debug on my cube project . only can one time program my chip.when disable debug on cube. i can program my chip.but cant debug .Cube version  4.17.0cubef1 : 1.4.0chip : stm32f103zc

Resolved! STM32L432 NUCLEO: bricked GPIO?

Posted on November 04, 2016 at 23:12Here's a little background. I run Arch Linux, and have been using the arm-none-eabi suite and openocd since early 2013 to program STM32s, first L1s and F4s, and now L4s. Except for vector.o from the appropriate li...

ARM chips programmers

Posted on November 25, 2016 at 09:46Hi guys, I view arm programmers and ti msp programmers.there is nest of chip in Msp's programmers(for unmounted chips).But ı have not found for arm chips.Can programmer board in below programed for arm chips?if th...

0690X000006037eQAA.jpg