STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2S Full Duplex Mode + DMA + HAL_Cube library

Posted on November 30, 2016 at 09:12Hello,In our application for audio codec IC, we have used I2S in full duplex mode with DMA.I have copied code for I2S . Can anyone suggest me what could be wrong with this ?static void I2SInit(){     // Enable PLL...

EXTI events vs interrupts

Posted on November 29, 2016 at 21:50Hello there, I am having hard time understanding what is the difference between external interrupt and external event. I was always using the former. I would appreciate if someone could point out the practical dif...

JTAG Pins ...

Posted on November 29, 2016 at 13:17Hello, I'm designing a board and I want to add JTAG on my board. If I use a following schematic, will it work ? (I'm using STlink-V2 as a programmer and a debugger.)

Mujtaba by Senior
  • 2104 Views
  • 3 replies
  • 0 kudos

CubeMX Feature Request

Posted on November 29, 2016 at 22:26Hello, I like CubeMX and would like to suggest a feature for the report generator. I use Nucleo boards a lot for development and small projects and the support for it is really great, but I always have to look up ...

valtin by Associate II
  • 1117 Views
  • 1 replies
  • 0 kudos

STM32F303 SPI clock in read processing

Posted on November 10, 2016 at 06:14I have question about SPI communication on the STM32F303. Read processing from slave device(SD) in SPI does not go well. I expected that 1 is returned, but 0 is returned. I check program code and signal by oscillo...

kenji by Associate
  • 1418 Views
  • 2 replies
  • 0 kudos

Stm32f1xx and can problem + bug on CUBEMX library

Posted on November 24, 2016 at 12:52Hi, i have a little problem on Can program.If you call HAL_CAN_Init and after HAL_CAN_Deinit, when you call again HAL_CAN_Init, the function ''HAL_CAN_Init'' return always Timeout on CAN1.Its a bug ?And i found th...

Marco1 by Associate II
  • 890 Views
  • 2 replies
  • 0 kudos

STM32F769 Discovery emWin Hello World

Posted on November 24, 2016 at 21:42Hi,I’m  trying to use the STM32F769I_EVAL STemWin_HelloWorld project on the STM32F769 Discovery. Cube: STM32Cube_FW_F7_V1.5.0\Projects\STM32F769I_EVAL\Applications\STemWin\STemWin_HelloWorldThe application runs on...

paul2 by Senior
  • 661 Views
  • 1 replies
  • 0 kudos

STM32F7 Discovery: Encoder Interface & Getting access to PA9

Posted on November 22, 2016 at 21:42Hello, I'm trying to get the encoder interface operational on the STM32F7 Discovery Board. Unfortunately, there seems to be a lack-of-pins problem. It seems like the easiest timer to use is TIM1. Channel 1 is on t...

jasonj by Associate
  • 905 Views
  • 2 replies
  • 0 kudos