cancel
Showing results for 
Search instead for 
Did you mean: 

External Crystal Connection

2013ee139
Associate II
Posted on June 27, 2016 at 19:40

Hello I am developing a evaluation board for STM32F427. I am connecting an external **RTC** IC (DS3231). Do i need to connect an other external oscillator for processor? Because in STM32F407 discovery board they have connected an external 8MHz crystal other than 32.768KHz which is used for **RTC**.

0

http://stackoverflow.com/questions/38059939/external-crystal-connection♯

Hello I am developing a evaluation board for STM32F427. I am connecting an external RTC IC (DS3231). Do i need to connect an other external oscillator for processor? Because in STM32F407 discovery board they have connected an external 8MHz crystal other than 32.768KHz which is used for RTC.

0

http://stackoverflow.com/questions/38059939/external-crystal-connection♯

Hello I am developing a evaluation board for STM32F427. I am connecting an external RTC IC (DS3231). Do i need to connect an other external oscillator for processor? Because in STM32F407 discovery board they have connected an external 8MHz crystal other than 32.768KHz which is used for RTC.

0

http://stackoverflow.com/questions/38059939/external-crystal-connection♯

Hello I am developing a evaluation board for STM32F427. I am connecting an external RTC IC (DS3231). Do i need to connect an other external oscillator for processor? Because in STM32F407 discovery board they have connected an external 8MHz crystal other than 32.768KHz which is used for RTC.

0

http://stackoverflow.com/questions/38059939/external-crystal-connection♯

Hello I am developing a evaluation board for STM32F427.

#!stm32-!clock #smt32f427
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 27, 2016 at 19:49

I'm not sure what the question is. How close is your design to that of the STM32F4-DISCO?

The F4 really needs an external HSE (High Speed, ie 4-26 MHz) source for USB and CAN to function within specifications.

A LSE source is needed for the F4 to come out of STANDBY via the internal RTC, you could presumably supply that as a single pin clock source if you don't want a second crystal for that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..