STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bad SPI clock duration in stm32f746

Posted on November 11, 2016 at 18:08Hello. I have got stm32f746 and I make project with cubeMX. I  want to use SPI4, SPI5, SPI6 as fullduplex master with 50Mb/s baudrate. Then I try to HAL_SPI_Transmit(&hspi4, pData, 1, 30000); in while(1) cycle. ...

ldpr by Associate
  • 1544 Views
  • 2 replies
  • 0 kudos

STM32F3 - Sending Sine Wave with DAC and DMA

Posted on November 29, 2016 at 05:51 Hello! I am currently trying to send a sine wave through the DAC. I've tried both using the std peripheral libraries and stm32cube, but to no avail. The frequencies and amplitude of the measured sine w...

kl4971tse by Associate II
  • 3447 Views
  • 4 replies
  • 0 kudos

How do I switch PLLSource once it is running?

Posted on December 07, 2016 at 22:19Hi, I want to start off my STM32F745VET6 running on the PLL sourced from the 16MHZ HSI oscillator. I need to run some I2C code to initialize an external multi-output high accuracy clock generator chip where one of...

STM32F042F6 SPI1 clock polarity problem

Posted on November 14, 2016 at 08:53Hello,On my currently developing device and I issued a problem. I'm using CubeMX 4.17, F0 package 1.6 and F4 package 1.13.1.I developed the code for F4 - SPI1 communicating with NRF24L01+ module using HAL library ...

help srf04 stm32f407

Posted on December 10, 2016 at 11:23hi allwhile (1) { int time; int i=0; GPIO_SetBits(GPIOA,GPIO_Pin_1); //delay_us(10); Delay(240); //Delay01ms(100); GPIO_ResetBits(GPIOA,GPIO_Pin_1); while(GPIO_ReadInputDataBit(GPIOA,GPIO_Pin_0)==0); while(GPIO_Re...

kakaducsy by Associate II
  • 1134 Views
  • 2 replies
  • 0 kudos

Debugging STM32F042 in Keil

Posted on April 11, 2016 at 23:05I have a problem with loading into debugger in Keil for STM32F042(Run to main() is off)- normal start for example from STM32F0xx_StdPeriph_Lib_V1.5.0\Projects\STM32F0xx_StdPeriph_Examplesfor STM32F030http://i.piccy.i...

chernobay by Associate II
  • 2107 Views
  • 4 replies
  • 0 kudos

Resolved! connecting STM32F4-discovery with Android through USB

Posted on November 29, 2016 at 17:45 Hello, I'm trying to connect stm32f4-discovery with Android phone supporting otg through USB virtual port. The microcontroller should work as device and smart phone will be the host. I used CDC library on stm3...

Is it possible to develop Packet analyzer or Network tap using STM32F2xxx?? Application is analysis of serial data. Suggestions

Posted on December 06, 2016 at 10:29I want to analyze the Serial data (UART) through STM32F2 series board (Nucleo 144). How one can develop Network Tap or Packet analyzer using Nucleo 144 Board. Any rough idea is most welcomed. Thanks in advance#stm...