STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f7 NOR flash ,

Posted on January 16, 2017 at 16:43A real simple questoin here, I'm  a hardware guy...sorry.Looking at the stm32F7 data sheets, and using the fmc in NOR flash mode. From the software perspective, would you have a lump of code that does the sequence ...

Proper way to use Cube_FW_ templates?

Posted on January 17, 2017 at 05:21How am I supposed to use these? I'm using SW32STM Workbench and can build projects from STM32CubeMX-generated code. I can build and run code from the Cube_FW_Fx examples.But when I try to copy the files from the Te...

Modify of HAL_PWR_EnterSLEEPMode() function

Posted on January 17, 2017 at 13:39I�m working on a time critical application with OpenSTM32 System Workbench for STM32 . I�d like to reduce the call time of HAL_PWR_EnterSLEEPMode(uint32_t Regulator, uint8_t SLEEPEntry). The code : void Sleep( uint...

eMMC in 8 bits Wide bus mode

Posted on January 04, 2017 at 15:35Hello,I'm using a STM32L4 and CubeMx to generate eMMC code, either the 8 bits wide bus mode configuration isn't supported and should be configured manually.I was able, with few code modification, to use the SD auto...

Spi dma: can't change spi prescale

Posted on January 16, 2017 at 16:10Hi,I'm trying to get spi driver working for ad-converter. Adc spi is supporting ~20mhz spi clock. Now my project APB2(Using spi1) clock is 84 Mhz and spi prescale is now 2( Spi clock is 42Mhz) and code is running f...

teijo by Associate II
  • 1706 Views
  • 2 replies
  • 0 kudos

STM32F429 Disco Timer ADC Trigger Problem

Posted on January 15, 2017 at 15:55Hi I'm trying to do an ADC Timer Trigger. What I want to do is trigger the ADC with 1kHz. To do this, I used Timer 2, ADC3 and DMA. I also activated the DMA Transfer Complete interrupt. The ADC is running in contin...

STM32 - PWM issue on TIM17...

Posted on January 16, 2017 at 18:28Hello,I am using a stm32f030k6t6 microcontroller and I have a problem with my pwm function on TIM17..It is very strange: when I power up my controller, sometimes my pwm act as PWM1 and sometimes as PWM2.I didn't co...

thomas23 by Associate II
  • 4757 Views
  • 9 replies
  • 0 kudos