2016-07-25 9:12 AM
Hello everyone.
1.) We are going to be using the STM32F437VIT6 in a new design and would like to get going with some firmware development. Is there a development / demo board that you guys could recommend that has the STM32F437VIT6 on it that would be compatible with the ST-LINK/V2?2.) For some bastic I2C, SPI and toggling pins do you think the Atollic IDE would be a good option?Thanks.-Mike2016-07-26 5:57 AM
Hi miller.mike.006,
I recommend you to the . You find firmware example in the package. You can, also, work and test the firmware using the All examples of previous Library package integrate four IDEs: EWARM, MDK, SW4STM32 and Attolic. You can select the one suitable for you. -Hannibal-2016-07-27 8:28 PM