STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM3221G-EVAL and SSD1963

Posted on December 04, 2014 at 20:09Hi:I am using the STM3221G-EVAL board and trying to use a a different TFT display than the original that came with the board. The original display is an Ampire display that uses a Ilitek controller ILI9320.The new...

eduardo2 by Associate II
  • 1288 Views
  • 1 replies
  • 0 kudos

STM32F4 ADC w/ DMA application notes & examples

Posted on February 24, 2017 at 17:09We are using the STM32F437 and I am trying to find application notes for using ADC with DMA. More particularly I would like to see notes or code examples where multiple channels (2) are interleaved. Thanks,jh

John Hite by Associate III
  • 2219 Views
  • 5 replies
  • 0 kudos

Large compiled application size, is this normal?

Posted on February 18, 2017 at 08:47Hi  I am just a beginner in the STM32, I have been designing for 8bit Freescale parts for years. I am using ST's Nuleo64 STM32L07 processor. Using STM32CubeMX I designed a very simple application that simply captu...

Simultaneous/synchronized start of ADC conversions without DMA

Posted on February 20, 2017 at 18:23The microcontroller i am using is a STM32F446.The STM32F446 is equipped with 3 ADCs.I would like to start one conversion of all 3 ADCs at the same time (simultaneous/synchronized start).I do not want to use DMA.I ...

Tob G by Associate II
  • 3037 Views
  • 4 replies
  • 0 kudos

IWDG short period (125 us) problem

Posted on February 23, 2017 at 13:04Hello,We are developing a PV converter and we have choose an STM32F407VGT microcontroller in order to controlling its power electronics and communications. We are using the ♯ in order to ensuring that the software...

STM32F0xx findings

Posted on November 14, 2016 at 22:07In a new project there are several identical STM32F031 devices in a role of a slave mcu, driving LEDs and reading in various input signals. As their functionality is very similar, it is tempting to have only one s...

Interleaved ADC

Posted on February 23, 2017 at 00:04Device: STM32F437I am using ADC3 channels 5 (rank 1) and 8 (rank 2) in interleaved mode, the input for channel 5 is 0 volts and the input for channel 8 is near upper limit. Trapping after the first interrupt the 3...

John Hite by Associate III
  • 1391 Views
  • 2 replies
  • 0 kudos