STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! fresh Custom HID Project, not flashable on my STM32F4

Posted on January 21, 2017 at 13:33Hey guys,I created 2 sets of projects with CubeMX for my STM32F429I-Disc 1 board.I project is a Device HID project, the other one is a Device Custom HID project.The Device HID projects works fine, the Custom HID pr...

Resolved! STM32L432 - I2C Address Off By 1-Bit

Posted on February 24, 2017 at 06:55 Hi, I recently brought up the I2C using the STM32CubeMx(4.0) and STM32CUBE_FW_L4_v1.6.0 and I was attempting to write to a slave device with an address of 0x2A. I noticed that my slave device was NACK-in...

0690X00000606OSQAY.png 0690X00000606OXQAY.png 0690X0000060678QAA.png
Nolan L by Associate III
  • 5984 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F303: GPIO configured with PP affect ADC readings

Posted on February 25, 2017 at 04:22Hi,I'm using a STM32F303 (landing page: http://www.st.com/en/microcontrollers/stm32f303k8.html) for one of my project. I have PA0 configured as a GPIO output with push pull used to turn ON/OFF a BJT. I also have P...

How to set stm32f407 sdio to 48Mhz?

Posted on February 25, 2017 at 17:25hi i want use sdio as 8bit mode and 48Mhz but i try to do this and i saw max 25Mhz on clk line for sdio port.how can i set sdio as 8bit-48Mhz mode?tnx for replay

eittinfo by Associate II
  • 1951 Views
  • 3 replies
  • 0 kudos

I couldnot make STM32F103RC CANBUS work

Posted on February 24, 2017 at 17:37hello dear forum,I copied following code from std peripheral libraryhowever I couldnot make it workwhat I am doing wrong ?thank you----------------RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);--------------...

Resolved! STM32F3 UART DMA problem

Posted on January 04, 2017 at 00:01 Hi,I am working  on an application on an STM32F303RET6 on a nucleo board. I am struggling to get DMA working on USART1 Rx.  I can successfully enable the USART port and it works correctly with the receive interrup...

STM3221G-EVAL and SSD1963

Posted on December 04, 2014 at 20:09Hi:I am using the STM3221G-EVAL board and trying to use a a different TFT display than the original that came with the board. The original display is an Ampire display that uses a Ilitek controller ILI9320.The new...

eduardo2 by Associate II
  • 1291 Views
  • 1 replies
  • 0 kudos