cancel
Showing results for 
Search instead for 
Did you mean: 

How can i send 0x00,0x07,0x08,0x0a,0x0d,0x1b using HAL_UART_Transmit??

SoHaeng.Lee
Associate II
Posted on September 24, 2016 at 11:37

hi

I'm using nuclei-f446re and LoRA communication module.

recently, i tried to send 0x00(null).

but i can't.

so i tried all all code send using LoRA comm module to another module. 

The result was not successful.

Not sent char : 0x00, 0x07, 0x08, 0x0A, 0x0D, 0x1B    (6 character not sent)

How can i send this character?

source code

------------------------------------------------------------------------

    

for

(n=0;n<=97;n++) sendData[n] = n;

    sendData[98] =

'\r'

;

    sendData[99] =

'\n'

;

    HAL_UART_Transmit(&huart2,(

uint8_t

*)sendData,100,1000);------------------------------------------------------------------------

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
LMI2
Lead
Posted on September 24, 2016 at 12:52

Can you send something else like text. I ask because it matters if you are able to send something or nothing at all.

Posted on September 24, 2016 at 15:26

Sounds like you might want to read the documentation for your LoRA module to understand how it actually works and what it expects.

I suspect that you need to look at how it ''escapes'' special characters, like you do in C '\n' or ESC ESC for other protocols.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..