STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is the minimum clock speed if I use ADC with DMA?

Posted on March 03, 2017 at 20:18I use STM32L151 for digitizing 3 values: Vrefint, Temp.sensor and 1 external source. Program uses sleep mode.I get garbage after switching CPU freq from 250 kHz to 4 mHz and correct values when switching from 500 kHz...

Resolved! Is I2C on STM32L4x6xx usable?

Posted on March 04, 2017 at 10:53Hi,I am trying to understand the errata sheet for STM32L4x6xx series of MCU (DocID026121 Rev 4, December 2016).I2C peripheral limitations section lists one of the silicon bugs as�2.6.3 Wrong data sampling when data s...

handle I2C bus error

Posted on March 03, 2017 at 07:45I have a problem with the i2c peripherie of a STM32f407.If i get a bus error the i2c is always busy.I try to solve this with a I2C_SoftwareResetCmd(I2C1, ENABLE), this works but then i cant start a new communication....

HSI/MSI calibration

Posted on March 02, 2017 at 12:55Hello,I'm developing my application based on the STM32L475.One of my goals is power consumption so I will set the STM32 to Stop1 mode.I have to work with UART and I2C so, to work in Stop1 mode I need the HSI16 to be ...

How to use USB as Mass Storage Class ?

Posted on March 01, 2017 at 22:17Everybody,How to use USB as Mass Storage Class ?This question is related with SDIO I had done intiating,Which configuration file do  I need to change ?I can see drive E on my computer now, but can not read the conten...

Resolved! hs usb stm32f429zi

Posted on March 01, 2017 at 15:17Hi,Does stm32f429zi support usb in hs mode? i found that PB 14 is required by USB-HS but on that pin red led is connected.Thanks for support.

John Doe1 by Associate III
  • 1285 Views
  • 3 replies
  • 0 kudos

Center aligned PWM

Posted on March 01, 2017 at 10:06 Hello, I need a 5-pulse modulation to attack two drivers with a resonant tank to create a sinusoidal. I have these 5 pulses created with DMA with TIM_CounterMode_Up, if I set them as TIM_CounterMode_Cente...

0690X00000602QzQAI.bmp 0690X00000602R4QAI.bmp

SHA256 RSA digest

Posted on March 01, 2017 at 22:48I have this working on a stmicroF427 part and I am trying to run the same code on a STmicroF103.  The only changes are that I used the M3 versions of the library on the F103 part, and the 427 system uses cube and the...

jim239955 by Associate II
  • 3277 Views
  • 8 replies
  • 0 kudos