User Activity

I'm porting some fully functional older CMSIS firmware to STMCube and TrueStudio. The old report is 363 bytes which compiles, but Windows Device Manager detects an error in the Report Descriptor. After some tinkering, setting USBD_CUSTOM_HID_REPORT_D...
Posted on October 02, 2016 at 20:39I have a very basic F103VET dev board, with the schematic. The board arrived running what I guess was ST-Link, which I don't use.  I was able to erase the Flash using the latest FlashLoader (FL) v2.8, via the Cmd l...
Posted on April 30, 2015 at 21:02I have two almost identical 72MHz boards which have code issues I suspect are related. I have DFU firmware that loads on to both boards, and both appear to the host as a USB DFU device. App firmware is loaded at 0x08...