STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 FOC SDK for stepper motor drive ?

Posted on March 25, 2017 at 06:55I've downloaded STM32 FOC SDK for testing closed lo loop stepper driving.Simply reviewing the API, I am not sure the FOC SDK is useful for closed loop control of stepper drive.For example, the shunt resistor configur...

Timer sync

Posted on March 24, 2017 at 17:44In RM0090 section 18.3.15 Timer synchronization all the master/slave examples use timers 1 and 2. Can only adjacent timers be used in master/slave modes, must the lower number be the master? I don't see where the cou...

John Hite by Associate III
  • 743 Views
  • 1 replies
  • 0 kudos

DMA2D Rotation

Posted on March 24, 2017 at 20:03Hi,The DMA2D peripheral is great, and I'm using with no issues.  I was wondering if it's possible to rotate an image 90 degrees using this peripheral.  Has anyone done this?Thanks!Bobby

Resolved! STM32F446 DMA Indexing

Posted on March 22, 2017 at 22:54I ultimately need 'instant on' ADC conversions.  For instance, when a timing gate goes high, I need to start taking ADC values immediately (the signal is only 100us wide),  The problem I'm running into is the lag: fi...

joesnyder by Associate III
  • 4712 Views
  • 6 replies
  • 0 kudos

UART variable length message

Posted on March 16, 2017 at 10:48Good morning, I'm making a program that should receive from the UART a variable length message. The message ends with '\n'I tried it with thisuint8_t rxChar=0;int main() {      HAL_UART_Receive_IT(&huart2, &rxChar, 1...

Resolved! STM32F407 : IWDG and erase flash sector

Posted on March 20, 2017 at 15:53Hi,In my application I'm using the Independent watchdog on a STM32F407 with a maximum reload period of 2 ms. During some maintenance operations, we need to save some configuration parameters in flash memory. Even if ...

Resolved! STM32L452CEU6 Availability?

Posted on March 24, 2017 at 02:08Are we getting close to the official announcement?  I recall reading that the L452's were supposed to be in the distribution channel this month.  Is that still the plan?  I see the part numbers are already there at a...