STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Transmitting and receiving data from DMX512

Posted on April 16, 2017 at 09:49We have used USART1 and USART2 for communication between STM32 and two DMX512 devices it is transmitting data properly but when using same USART for receiving data from DMX512 it is not working properly. When i use d...

line level audio out?

Posted on June 05, 2016 at 15:42I'm using the STM32F746G to play with some audio DSP stuff and it's working fine with headphones but when I connect the output to external amps I get whine and low signal level.  I'm using the OUTPUT_DEVICE_HEADPHONE ...

dennis by Associate II
  • 1893 Views
  • 3 replies
  • 0 kudos

gestures working with ft6x06?

Posted on April 16, 2017 at 21:10f7 cube 1.6.1, stm32f769i_discovery board.No matter what I do, I cannot seem to get this controller chip to return a gesture ID. does this chip actually support swipes or not? The documentation says it does, the driv...

stm32f103c8t6 spi communication with Arduino

Posted on April 15, 2017 at 11:42Hello I devolved a code for stm32 as a master and for arduino as a slave , to send a byte through SPI.But it did not work. I want to know what is the wrong in my code.STM32 Master Code :static void SPI_Config(void);i...

how to capture picture with stm32f4

Posted on April 16, 2017 at 11:35Hi everyone;I want to capture picture with stm32f4, I found some website take video however I am new at using stm32f4 thus I cannot rewrite this keil program, could you help me at this issue pleasemy founding website...

We have SRAM FSMC configuration code available for STM322xG in cubeF2, I want to implement Muxed NOR with the help of same code

Posted on April 15, 2017 at 13:55Hi,As the title I want to implement Muxed NOR on STM32F207ZG Nucleo boardfollowing is SRAM read write code. for (uwIndex = 0; uwIndex < BUFFER_SIZE; uwIndex++) { *(__IO uint16_t*) (SRAM_BANK_ADDR + WRITE_READ_ADDR + ...

Activate both CAN 2.0A and CAN2.0B in the same time

Posted on April 14, 2017 at 18:23Hello ALLIn order to perform a new project using STM32F302VC micro-controller . I have a question , :it s possible  to activate the CAN controller in standard and extended configuration (CAN 2.0A and CAN2.0B) in the ...

STM32F0 ADC DMA Assistance

Posted on April 14, 2017 at 21:19Hello All,Hoping someone can help me understand the ADC DMA via ST's HAL. I haven't been able to locate the information I need to understand how it works or what I have read still doesn't give me what I need so if so...

0690X00000606moQAA.png

how to read multi channel ADC ?

Posted on December 30, 2016 at 13:53hi , i am using STM32fo with cube mx and keil mdk5. in my project i have to read muti channel ADC value . For this when i used DMA  , DMA has its interrupt and in my project i already used timer interrupt so these...