2016-11-20 2:59 AM
Hello!
I post this subject because I have some problems to communicate with my BMP I'm using SPI protocol and configured it like this:spi_card.Instance = SPI2;
spi_card.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64;
spi_card.Init.CLKPhase = SPI_PHASE_1EDGE;
spi_card.Init.CLKPolarity = SPI_POLARITY_LOW;
spi_card.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
spi_card.Init.DataSize = SPI_DATASIZE_8BIT;
spi_card.Init.Direction = SPI_DIRECTION_2LINES;
spi_card.Init.FirstBit = SPI_FIRSTBIT_MSB;
spi_card.Init.Mode = SPI_MODE_MASTER;
spi_card.Init.NSS = SPI_NSS_SOFT;
spi_card.Init.TIMode = SPI_TIMODE_DISABLE;
spi_card.Init.CRCPolynomial = 7;