STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F446: SAI1-B and UART4 simultaneous usage problem

Posted on May 23, 2017 at 14:17Hi there,i have the following issue:Part: STM32F446VHAL: Cube32MX, Version 1.16.0I use SAI1-A with an ADC to sample audio signals (Stereo, 24Bit, 24kHz).An Audio-DAC is connected to the SAI1-B. The SAI-B generates a wa...

STM32F103 RCC HSE Problem in Stm32cubeMX v4.21

Posted on May 22, 2017 at 19:15Hello ,I designe my project using STM32F103RBT6 with 8 Mhz external crystal , and im using STM32CubeMX  4.21 .when i select HSE in RCC i have problem. when i debug the program , i have problem here:RCC_OscInitStruct.PL...

GDB Server on Win10

Posted on May 21, 2017 at 12:02Hello community,I have an error (Couldn't find any ST-Link/V2 devices) on Win10 environment. No USB3.ST-Link Utility (GUI & CLI) works fine, Mass storage too. What is not working is the https://www.emb4fun.de/archive/s...

Timer2 Configuration

Posted on May 15, 2017 at 10:47I'm working on STM32 nucleo432lkc. I'm trying to divide the MSI frequency for the timer by 50 but when I try this , i get nothing on the ouput of the pin. Below is the timer 2 code :void TIM2_init(void){      TIM_Clock...

DOSS FOF by Associate II
  • 4333 Views
  • 10 replies
  • 0 kudos

osxAcousticBF Software Library example no output sound

Posted on November 15, 2016 at 14:18Hi. I was setup osxAcousticBF Software Library, import example to SW4STM32,But can not listen any output sound.Ac_SL is operate here OK. I can listen sound via USB and receive source azimuths. #open.audio-softw...

Evg Cha by Associate II
  • 2912 Views
  • 6 replies
  • 0 kudos

ST32446-EVAL doesnt support SW4STM?

Posted on May 18, 2017 at 17:17Hi, I cannot dbg and programming stm32446e-eval board using onboard st-link, pic below. I checked also other board stm32f769i-disco and its working fine on the same enviroment. Log:Unplugged target or STLink already in...

0690X000006072mQAA.png
embvis by Associate III
  • 3138 Views
  • 7 replies
  • 0 kudos