STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BSP library failed to link with HAL library

Posted on June 28, 2017 at 17:51I use BSP/STM32469l-Discovery (from STM32CubeMx) , and use STM32F4xx_HAL_Driver to do a small project like this video : https://www.youtube.com/watch?v=u_TVAudWabI  (I convert evaluation board from STM32F429-Disco to ...

Dai chou by Associate
  • 2829 Views
  • 4 replies
  • 0 kudos

STMF746 CAN1 Setup

Posted on July 10, 2017 at 23:56Good Afternoon! I need help configuring an STM32F746 nucleo board for use with CAN1.  I am using PCAN view to send CAN messages at 250 kBit/s, and CubeMx to generate the initialization code. I am sort of new to this a...

0690X00000607OLQAY.png

The problem with receiving signals by SPI

Posted on July 10, 2017 at 17:26Hello.I want to connect an electronic micrometer to the microcontroller stm32f103�?8t6. The electronic micrometer has 2 outputs (date and clk). Judging by the readings of the logical analyzer, this is similar to the S...

STM32 RTS

Posted on July 10, 2017 at 15:42The STM32F437 USART has an automatic flow control feature.  My understanding of this is that CTS and RTS will be handled automatically by the MCU.  My interest is in RTS.  To me it seems that RTS is asserted/de-assert...

CubeMX and LwIP (DP83848)

Posted on May 25, 2017 at 21:20We now have CubeMX version 3.20 Tried to make a project for the 407 but no support for the DP83848 ??Can somewhere share an example project using CubeMX and LwIP

Resolved! EXTI minimal pulse length clarification

Posted on April 25, 2017 at 14:11DS STM32F405xx STM32F407xx, DocID022152 Rev 8, Table 50. I/O AC characteristics :tEXTIpw Pulse width of external signals detected by the EXTI controller  - min.10nsThis hints that there's a pair of edge-sensitive lat...

STM32F769I Discovery board LCD interface

Posted on July 10, 2017 at 15:07I have gone through all of the tutorials above and i also have the stm32f4 discovery kit on which  I am able to implement all of the peripherals using cubemx and (Keil or Eclipse).  The problem I am facing with the ST...

STM32F103 SPI Slave connection Bug?

Posted on July 10, 2017 at 09:59Hi,      According to the RM0008.pdf , when spi in slave mode the MISO pin is transmit data, the MOSI pin is receive data.   But according tests and the exampleSTM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPerip...

0690X00000607WNQAY.png
cap vor by Associate
  • 1252 Views
  • 1 replies
  • 0 kudos