STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeL0 - USB example for STM32L073RZ

Posted on July 17, 2017 at 16:17Hi,I'm developing a bridge USB-SPI with a STM32L052 microcontroller. In this starting moment I'm developing the same application using the evaluation board STM32L073RZ. I'm using SW4STM32 IDE and STM32CubeL0 software....

STM32 ST Link Utility

Posted on July 14, 2017 at 03:30Hello, I'm using STM 32 ST-Link Utility to program my MCU. I want to make sure that when I program the board multiple times I don't erase the data saved in a particular page on memory? Can I do that? If so, then pleas...

Tkamaal by Associate II
  • 1488 Views
  • 2 replies
  • 0 kudos

Resolved! HAL_I2C_Master_Transmit() ''too few arguments''

Posted on July 18, 2017 at 05:08Hello, I'm new with STM32 and this is the first time for using I2C on STM32.My environment is Keil5+cubeMX4.22.I can make the config by cube and I wrote following code, but couldn't compile it.uint8_t c[5] ={'a', 'b',...

Need STM32L4 IOT Discovery Kit full Webinar access

Posted on May 16, 2017 at 17:08Participated in the webinar from the ST Microelectronics broadcasted emails. Invested most of the hour listening through the Milli Vanilli reborn presentation on how to use the AWS with the new STM32L4 IOT Discovery Ki...

Mon2 by Senior III
  • 1975 Views
  • 8 replies
  • 0 kudos

RCC HSE CONFIG

Posted on July 17, 2017 at 07:01heyI'm use stm32f013cbtx and 8MHz crystal connect to HSE And use standard peripherals library with Keil v5.How can i config micro-controller for 72 MHz clock(with Cmsis)?is it possible?Thanks

Problem receiving data from CC2540

Posted on July 13, 2017 at 18:28Hi,I have an STM32 and am trying to receive a single byte of data from a CC2540 over UART. I've verified that the data transmission from the CC2540 is working properly (I can receive the data in a serial terminal) but...

How to calculate I2C SCL Speed

Posted on July 14, 2017 at 06:27I'm trying to get a 100 or 400 kHz rate on I2C3 SCL to interface with a Sparkfun IMU breakout board. I was wondering what value I should set 'TIMING' to in order to achieve this rate with an STM32L476RG Nucleo board. ...

RTC can't work because PLL already use

Posted on July 17, 2017 at 07:46Dear Sir:I had reference the PWR_STANDBY_RTC sample code form STM32Cube_FW_L4_V1.8.0This sample code are work well and wake up about 30 second,but after move to my code get return fail atif(HAL_RCC_OscConfig(&RCC_OscI...

Resolved! HAL I2C Communication Problem

Posted on July 14, 2017 at 11:52Dear Sir/Madam,I am working on STM32F405 mcu.I developed my code on cubemx and HAL drivers.I want to interface microchip adc 'MCP3428' via HAL I2C drivers but unfortunately i was failed.Anybody of you please help me t...