STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Floating point instructions

Posted on August 17, 2017 at 15:16I am using STM32F303VC with System Workbench IDE.I can't for the life of me get the hard floating point option to work. The compiler never generates floating point instructions. It' only generating soft code with li...

Virtual COM Port Trouble

Posted on August 11, 2017 at 00:03Fedora 25 (64 bit)STM32F746G Discovery boardI've been able to program the board using a simple Makefile project.  The board flashes and runs the program, in this case, a LED flasher that has code to send messages to...

CAN messages filtering

Posted on August 15, 2017 at 14:16Hello,I have been developing control software based on STM32F207 and I have been using CAN interface for communication. There are several messages with different IDs on the CAN bus which my software is interested in...

Ethernet Initialisation

Posted on April 13, 2017 at 07:38Hi guy's...I configured Ethernet in STM32f429zi controller using STM32cub max software, And auto code is generated in Keil IDE,  Next i don't know how implement a code?please help me any body,It's urgent . 

QSPI Receive

Posted on August 18, 2017 at 19:28I am using a Nucleo-144 board with a STM32F413.  I have a PmodSF3 NOR Flash (Micron N25Q256A) attached.  I am trying to communicate using QSPI.  I have a logic analyzer attached and can see that I am talking to the ...

stm32f334 for MCU for the digital power?

Posted on August 18, 2017 at 15:22Hello!I am evaluating MCUs for advanced power supplies. The MCU should become our standard MCU for the digital power conversion applications. We typically have an (interleaved) buck, a full/half bridge and a synchro...

T B by Associate II
  • 1038 Views
  • 1 replies
  • 0 kudos

STM32H7 evaluation boards for testing DCMI?

Posted on August 13, 2017 at 01:10Would it be possible to test the DCMI interface using the evaluation boards that are currently available? The H7 series has an enhanced DCMI controller compared to the previous products. But  H743, H753 boards don't...

M. Jeong by Associate II
  • 1135 Views
  • 5 replies
  • 0 kudos

ETM Trace problems with newer STM32F7 derivates

Posted on August 18, 2017 at 11:38Hello,is it possible that the ETM Trace does not work correctly in newer STM32F7 derivates?In a first revision of our controller board, we used STM32F746ZGT. Here it was possible to use the ETM trace with a CPU spee...