STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

B-L072Z-LRWAN1, CubeMX project

Posted on August 23, 2017 at 11:11Hi.I am analyzing with B-L072Z-LRWAN1.If you have a CubeMX project file, it will help you analyze it.Can not convert AT_Slave project to CubeMX project?Clock, and LPUART settings.Please.

Jin ho An by Associate II
  • 1525 Views
  • 3 replies
  • 0 kudos

STM32L1xxx Firmware Over The Air

Posted on August 24, 2017 at 06:35Hello everyoneI have a little problem to get help from everyoneI'm working on FOTA using the STM32L1, after loading the bootloader and the application (using Jlink v9 programer), the mcu runs normally. If I download...

Unknown STLink JTAG/SWD mode?

Posted on August 24, 2017 at 04:50In STLink settings menu we can chose JTAG or SWD but which JTAG and SWD mode is it?Full SWJ (JTAG-DP + SW-DP) - Reset StateFull SWJ (JTAG-DP + SW-DP) but without NJTRSTJTAG-DP Disabled and SW-DP EnabledTrying to fig...

stm32f4 bad sdio throughput

Posted on August 23, 2017 at 17:55Hi,I'm using an STM32F446 @ 168MHz.APB2 Frequency = 84 MHzSDIO_CK frequency = 12MHz @ 4-bit lines = 48 Mbit/secShoud give a reading throughput of approx 6MBytes/sec.But using ST's SPL, reading 1 block ( of 512 bytes...

Kuikui by Associate III
  • 2984 Views
  • 5 replies
  • 0 kudos

STM32F071RB6T ADC FAIL ?

Posted on August 23, 2017 at 16:03Hey,i have a strange behavior of STM32F071RB6T.I initialize the RCC, TIM3 for PWM 1Ch. works!I initialize the RCC, TIM3 for PWM 1Ch, ADC with DMA. works!I deaktivate PWM init and just whant to test the ADC with DMA ...

Resolved! FMC and 16/32b multiplexed mode

Posted on August 23, 2017 at 17:23Hello,I have some doubts with understanding and configuration of specific FMC modes. May I kindly ask you to check if my intentions are correct?We have STM32F767 connected to our proprietary memory-mapped periphery ...

dstindl9 by Associate II
  • 1403 Views
  • 1 replies
  • 0 kudos