STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

problem with programing aplication

Posted on November 27, 2015 at 09:26Hi all, I have a problem with programing STM32L15V. I am using about 1m long connection to device from ST Link V2. When I am using STM32 ST-LINK Utility (V3.7.0) there is no problem with connection/programing/e...

Resolved! STMCube QSPI ExecuteInPlace Example

Posted on October 11, 2017 at 21:49Hi,The STM32CubeMX repository has discovery board example projects for using QSPI flash.These example projects extern two variables:#if defined(__CC_ARM)extern uint32_t Load$$QSPI$$Base;extern uint32_t Load$$QSPI$$...

DMA issues for injected channel in ADC multimode

Posted on July 12, 2017 at 01:30Dear community,I have some issues to  make my STM32F446 work properly. I would like to use ''triple combined regular simultaneous + injected simultaneous mode''. The aim is to use the 3 ADCs, each measuring 1 regular ...

0690X00000607TQQAY.png 0690X00000607YdQAI.png

Nucelo STM32F429ZI with 8742A PHY

Posted on October 10, 2017 at 22:34Hi,I am using the latest ST32CubeMx Ver. 4.22.Creating a new project with the wizard and selecting my target board Nucelo STM32F429ZI.When selecting the middleware ETH connectivity I have DP8348 as only choice wher...

STM32L071 DMA from Mem to Peri

Posted on October 11, 2017 at 14:33Hi,I want to use DMA for transfer data from memory (uint16_t DMA_BUFF[10]) to register TM21.ARR. I want to use TIM6 for generating events every 50 ms for DMA to transfer DMA_BUFF[xx] to TIM21.ARR.In First 50 ms I w...

JAN R by Associate III
  • 1704 Views
  • 5 replies
  • 0 kudos

Hard Fault with ''STemWin_HelloWorld'' Example.

Posted on October 11, 2017 at 04:05Compiler:           IAR Workbench v8.11.3Graphics:           STemWinHardware:          STM32746G Discovery BoardHAL Version:     V1.8.0Demo Project:   C:\STM32Cube_FW_F7_V1.8.0\Projects\STM32746G-Discovery\Applicat...

ç�?¨STM32F765芯片外部能扩展2片8ä½�å�•颗256Mbçš„SDRAMå�—,怎么连接呢?

Posted on October 11, 2017 at 10:28请问ç�?¨STM32F765芯片外部能扩展2片8ä½�å�•颗256Mbçš„SDRAMå�—,怎么连接呢?

1 1 by Associate
  • 692 Views
  • 0 replies
  • 0 kudos