cancel
Showing results for 
Search instead for 
Did you mean: 

Evaluating SPWF01SC for file transfers

jm4ck3nz13
Associate II
Posted on August 31, 2017 at 00:52

Hi Everyone,

I've been evaluating an SPWF01SC to see whether it's suitable to add web browser file transfer functionality and a control interface to an existing embedded (bare metal) project.

Host controller is an STM32F429 and files are stored on an SD card. Over USB this appears as a drive in Windows; I'd like something similar on the wifi interface. File sizes are < 2MB, most are a few KB so I can live with the relatively slow transfer rate (I've done some benchmarking using sockets).

As I'm not very familiar with web servers can the module can do this out-of-the-box with minimal coding (i.e. I'm missing something)? Is it better to bypass the web server and use sockets in the host (this is hard, I know)? Is the module just not suitable at all? Is there a better way?

Many thanks.

#spwf01sc
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0