STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

sdio and fatfs r0.12 not working

Posted on November 09, 2017 at 20:55Hello!i have very simple project on board stm32f4discovery, it is test microSD card project, code was generate in stm32cubemx version 4.22 (fatfs r0.11) with pack STM32Cube_FW_F4_V1.15.0 for MDK-ARM V5. This proje...

The strange work of SPI

Posted on December 07, 2017 at 11:37 I use STM32F401CBU6 with two AD7690 in chain mode (Page 21: http://www.analog.com/media/en/technical-documentation/data-sheets/AD76pdf). I connected IN AD7690 to VREF. The oscilloscope I get 11111111 111111...

0690X0000060PGPQA2.jpg

Encoder mode both edges

Posted on March 31, 2016 at 17:02Hi to everybody!I need some help to correct this code. It seems to be correct, but it counts only 8 edges per cycle, while I need to take into account all the 16 edges that are avaiable (rising and falling, 4 sensors...

STM32F767 LQFP100 in standby, but core regulator stays on

Posted on August 24, 2017 at 12:20I am trying to get the STM32F767 in the LQFP100 package to go into standby but the internal 1.2v regulator stays on.There is a complication in that it uses external oscillators while running, but for shutdown I swit...

Gid Rid by Associate II
  • 1328 Views
  • 3 replies
  • 0 kudos

STM32F429 Discovery OverCurrent LED

Posted on November 07, 2014 at 23:26Hi everyone.I'm not sure what I did, but my F429 Discovery board is drawing way to much current. The overcurrent light (LD6) turns on when I supply the board with power and U8, which I believe is a power distribut...

stone by Associate II
  • 1635 Views
  • 2 replies
  • 0 kudos

How wake up from I2C when I enter STOP mode?

Posted on December 07, 2017 at 05:59Thx for reading,I am using I2C of STM32L476, and have one Master , two Slave device.Slave1 will go into STOP mode, and need wake up by I2C.Slave2 not be polling by Master every 100ms.But after Slave1 into STOP mod...

0690X000006095iQAA.png

STM32f373 SDADC multi channel error.

Posted on December 07, 2017 at 05:43Hi, I use 3channel of SDADC in injected mode.My error is SDADC value is saved anothor variables.SDADC1 result -> saved at SDADC2 variable.SDADC2 result -> saved at SDADC3 variable.SDADC3 result -> saved at SDADC1 ...

HAL_SPI_Receive never returns by timeout

Posted on December 06, 2017 at 23:27Hello everybody! I'm trying to implement some examples using the hal spi library in the B-L072Z-LRWAN1 (LoraWAN Discovery Board). This board has a STM32LO on it, and I'm trying to implement spi communication with ...