STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4: How can I move code into fast RAM?

Posted on December 31, 2017 at 10:23So far I've been using the STM32F722, but I'm planning to switch to either STM32F446 or STM32F429.On the F722, I moved speed-critial code to ITCM RAM. The F4s don't have ITCM RAM, but an ICache and/or CCM. How do ...

IAP and External flash

Posted on December 29, 2017 at 04:46I have 2 questions -Q1:Can IAP be used to update the internal flash from an external flash.  Here is what I want to do:   1) Download code to the External flash from a remote location.  Such as Wifi OTA   2) Have ...

jeff belz by Associate II
  • 1289 Views
  • 2 replies
  • 0 kudos

STM32F4 USB to PC communication

Posted on December 31, 2017 at 10:35Hi,I am using STM32F405 mcu.now i want to interface my STM32F405 usb with PC  win32 & win64 bit os.I dont want to use any converter IC for same.Thank you.

STM32 with integrated phy

Posted on September 25, 2015 at 12:28Hey, is there an STM32 device which would have an integrated phy and would only require an RJ45 jack for LAN interface? I tried to look for it, but I could not find it.

matas by Associate II
  • 2756 Views
  • 4 replies
  • 0 kudos

STM32L432 - HSI16 accurate enough for use without crystal?

Posted on December 30, 2017 at 16:23I started designing a product with a STM32L432KCU6. Looking at the datasheet I noticed that the HSI16 clock seems to be very accurate. From Figure 14, p 95, it seems that the clock is pretty much within 16MHz +/- ...

mluessi by Associate II
  • 1955 Views
  • 3 replies
  • 0 kudos