STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN and system clock configuration

Posted on April 26, 2017 at 06:50Hi, CAN interface  on STM32F769I is not sending data using Clock configuration 1 but CAN interface is sending data with configuration 2. I am not able to narrow down that how the CAN interface is getting affected by ...

Jith cr by Associate II
  • 1758 Views
  • 3 replies
  • 0 kudos

Resolved! H743 ._user_heap_stack in D2 section causes Hard Fault

Posted on January 03, 2018 at 22:16Hello.Why is it not possible to point the ._user_heap_section in the D2 RAM section?A tiny project based on SW4STM32 for NUCLEO-H743ZI is attached.I just modified the linker script to have _user_heap_stack in D2 an...

STM32f030rc AES Encryption

Posted on January 06, 2018 at 08:21Hello everyone,I am using STM32f030rc for my application. In which I want add 128bit AES encryption. For that I am referring STM32_Cryptographic _Examples. I have taken functions from AES128_CTR file. In which I am...

How do I enable UART4 on the B-L475E-IOT01A? It appears that UART4 needs to be defined; but in which header file. What else needs to be done to enable and use the port?

Posted on January 07, 2018 at 06:35I desire to use UART4 to talk to a GPS module over serial communications on an Arduino shield board. To do this I need to use UART4, but it does not appear to be enabled. 

How to stop HAL_CAN_ErrorCallback

Posted on April 25, 2017 at 20:27My hardware has to disconnect the CAN bus sometimes. When i do the callback HAL_CAN_ErrorCallback will pop up. My CAN bus has to continue work so i clear all flags that i found:__HAL_CAN_CLEAR_FLAG(hcan,CAN_FLAG_EWG)...

Nucleo-L432KC store data in Flash using mbed

Posted on December 15, 2017 at 05:11Hello,I am using my Nucleo-L432KC for a project and my client wants to use mbed online compiler. I am trying to save some variables into the flash memory (because there is no EEPROM) and unfortunately there is no ...

Duy Tran by Associate II
  • 4772 Views
  • 9 replies
  • 0 kudos

Building samples of STM32CubeF7

Posted on November 14, 2017 at 14:13I'm new in this forum. I've got STM32F779I Eval board for one of our product. I've installed STM32CubeF7. I've also installed System workbench for STM32. Then I tried build one of the sample and could not build, i...