cancel
Showing results for 
Search instead for 
Did you mean: 

I am looking for stm32f407vg discovery board's default program(PC mouse)

m m
Associate II
Posted on September 01, 2017 at 09:11

Hi,

I am looking for discovery default program that acts like computer mouse. if there is better program to using gyro and accelerometer sensors of the board, I will be happy to see and learning from them. 

#mems-accelerometer #stm32f407vg-discovery
This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
Nesrine M_O
Lead II
Posted on September 04, 2017 at 10:31

Hi

hamintouri1

,

Please try to have a look to the demonstration example under the STM32F4 cubefirmware package

STM32Cube_FW_F4_V1.0\Projects\STM32F4-Discovery\Demonstrations

-Nesrine-

Posted on September 07, 2017 at 07:33

Hi Nesrine,

May you explain more about cube? I can not understand what it is? and especially it's relation to CMSIS?

Posted on September 07, 2017 at 07:37

Also where can I find the pad '

STM32Cube_FW_F4_V1.16.0\Projects\STM32F4-Discovery\Demonstrations' ?

Posted on September 07, 2017 at 09:18

Hi

hamintouri1

,

-Nesrine-

Posted on September 08, 2017 at 07:31

I have downloaded STM32cube, and went to demonstration and wanted to build the project but it says:

The following Device Family Pack(s) are required by the project:

Keil:STM32F4xx_DFP:2.11.0

And when I push install button below the message it says: ' one or more Device Family Pack Device are not present, would you like to choose another device?'

m m
Associate II
Posted on September 08, 2017 at 11:07

I have another question. if I want to convert the demonstration MEMS project to LL project, what is the true way?

Posted on September 08, 2017 at 09:54

Hi

hamintouri1

,

Could you please try to download directly theMDK5 Software Pack (

STM32F4xx_DFP:2.0)

from this

https://www.keil.com/dd2/pack/

0690X00000608AcQAI.png

-Nesrine-

Posted on September 08, 2017 at 11:05

Thank you Nesrine,

But I chose to select another device and I did select 'stm32f407vgtx' from 'software packs'. and problem solved and I built the project and ran it OK. 

So, did I do a wrong way? Should I download the package you put? what is that? 

m m
Associate II
Posted on September 10, 2017 at 08:58

The accelerometer by this example works fine, but it doesn't act as computer mouse!