STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DS18B20 HAL lib for STM32F0

Posted on January 23, 2018 at 14:33Hello,I have been looking for a library for the ds18b20 compatible with stm32f0 and with the HAL driver but without success, so I decided to modify old one to make it compatible.this lib uses while loop delay, the ...

RTC + STM32L NUCLEO + Contiki

Posted on January 23, 2018 at 10:37I found a strange behavior of the STM32L NUCLEO cards. I installed a sensor network using Contiki and I implemented an RTC. If I try to set RTC_SYNCH_PREDIV to a value above 1023 (for example 2047, 4095, ... up to ...

simval986 by Associate II
  • 1066 Views
  • 1 replies
  • 0 kudos

stm32f407 -- PINRSTF is set after power cycle

Posted on January 23, 2018 at 14:43Should the NRST external reset (PINRST) be set on an STM32F407 after a power reset?I want to be able to count the number of each type of resets in my code. The problem that I have is that the NRST pin reset is alwa...

dibs by Associate II
  • 936 Views
  • 0 replies
  • 0 kudos

I2C comm issue between MCUs

Posted on January 23, 2018 at 12:57Hi,I am using I2C to send data between two STM32F4 MCUs with the same MCU working as a Master always. The master MCU controls a display and sends the slave a massage just when the user changes a parameter.I am usin...

DMA with ADC Injected mode/stm32f4

Posted on January 19, 2018 at 15:52hello, I'm working with the stm32f4-discovery Board , in fact i have a problem using the DMA with an ADC 'injected channel'. I've configured the DMA to transfer the converted data from the injected data register 'J...

stm32cubemx V4.23.0 bug report.

Posted on December 18, 2017 at 07:18when used the 103 series MCU,  the SWD port will been disabled in follow step.1) enable the SWD interface. 2) enable tim3 CH1 PWM function and remapping the output pin to PB4. 3) when the tim3 init code run to __H...

Bruno Hu by Associate II
  • 1252 Views
  • 2 replies
  • 0 kudos

IAP jump to APP, but it don't work.HELP!!!

Posted on January 17, 2018 at 11:38Hi,I was doing IAP&App in STM32F030rc. When I finish IAP and APP, and run from IAP to jump to APP, it can not be realized. I have try many ways, but useless. Please help me, I have waste a lot of time for this func...