STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F334 with 24C32 EEPROM I2C Read/Write

Posted on February 22, 2017 at 09:59 Hi, Trying to get I2C communication between a F334 and a 24C32 EEPROM working, The read and write functions do return correctly, but the reads do not match what has been written to the EEPROM. Struggling t...

Trouble with “P-Nucleo-Azure 1� kit: not able to recogbize expansion board X-NUCLEO-IKS01A2 (''#ifndef IKS01A2''). Has anyone already had such a problem?

Posted on February 22, 2018 at 10:11Hallo everyone,I am working with the hardware kit �P-Nucleo-Azure 1� (STM32 Nucleo Pack for IoT node with Wi-Fi, sensors and NFC Connected to Azure cloud) and am having troubles in making it work.I have imported t...

Update STM32L073 programmcode

Posted on February 21, 2018 at 17:27Hey, I am facing a specific task and I could really need some help with that. So I have many stm32L073 µC which all run the same programm. The programm has a stored list of constants in them which are used while ...

Resolved! How can I use USE_DMA_TEMPLATE in stm32cubemx?

Posted on November 21, 2017 at 03:40I use stm32cubemx version 4.23. When I use SDIO 4bit and FATFS middleware, I see USE DMA Template option. If I choose 'disable', my code will run correctly. But If I I choose 'enable', I can't read and write data ...

STM32F429-NUCLEO-144 UART3 IS NOT RECEIVING

Posted on February 21, 2018 at 04:06 Hi, I amUsing STM32F429-NUCLEO- I write the code for UART3 transmit/receive (poling method) and the board is transmitting but the data is not receiving. Pls help me to fix the issue. Find the attached source...

pratheep by Associate II
  • 7869 Views
  • 22 replies
  • 0 kudos

Advice to handle data between Timer IRQ and DMA USART TX IRQ

Posted on February 22, 2018 at 07:46Hello,i am working on a project where i read 4 external adc's in a timer irq and i need to send the data very fast via usart.I know this is achievable only trough DMA USART TX request.The timer irq is executing on...

Bogdan by Senior
  • 735 Views
  • 0 replies
  • 0 kudos

Advice of hardware and software for STM32

Posted on January 14, 2018 at 07:03I am new to this group and wish to start using the STM32 group of MCUs. There seems to be a lot of choice here. Can someone recommend what hardware/software to use in my development. I have used MCUs from Microchip...

martech by Associate II
  • 4764 Views
  • 10 replies
  • 0 kudos