2017-11-01 4:54 AM
Hello,
device headers of new release STM32Cube_FW_F2_V1.7.0 still have defines like
#define GPIO_AFRH_AFSEL13_1 ((uint32_t)0x00200000U)
I reported this misuse for uint32_t in the headers several time, with most other headers removing the superfluous and harmfull 'uint32_t'. Does the F2 header team not care about problems reported to other teams?
Otherwise F205 and F207 still reports a HASH_RNG_IRQ
HASH_RNG_IRQn = 80 /*!< Hash and Rng global interrupt */
} IRQn_Type;while the Hash is non-functional in F205/F207.
2017-11-01 9:13 AM
A closer look shows that only F7 and H7 do not use #define and a unistd.h types together, probably as they where created after my first report.
2017-11-02 1:43 AM
Hi
Bonnes.Uwe
,I agree with you that the best practice is to check a reported issue/bug across all families/packages.
Unfortunately, sometimes there is a miss.
These 2 issues are highlighted again to be fixed in new package version. Thanks for help.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.