STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help with selection of external memory.

Posted on March 29, 2018 at 11:25I am using DCMI peripheral to drive camera modules. At this point, I am able to obtain images with 320x240, 16 bits/pixel. I am working with a display connected via FSMC to the MCU and the display already provides en...

Running a 3.3V STM32F0 on 6.5V

Posted on March 31, 2018 at 19:35I'm using an STM32F0 in a high volume low power project running on a LIR2032 that can be charged via USB. The STM is specd at 2.4 - 3.6V, with 4.0V as the absolute maximum. When the battery is fully charged however t...

PB13 PiN of STM32F429 for CAN2

Posted on April 01, 2018 at 19:13Hello, First of all, I am sorry for my english. Then I am doing a application with CANBUS Protochol. so ı need to use PB13 pin of STM32F429. but when I use this pin, CAN2 is not work. When I look datasheet, this pin...

STM32F030 eeprom emulator

Posted on March 23, 2018 at 13:58HI I'm lookin for a eeprom emulator for a stm32F030 cpu,and if I go to : https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libr...

spa23 by Associate III
  • 1621 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F051 10xPWM signal capture

Posted on March 31, 2018 at 22:59Hi guys!I use HAL drivers and I would like to measure the duty cycle of 10 x 25 kHz (asynchronus) PWM signal, but I'm not sure which peripheral should I use:- if I use timer with capture mode then I get 2 x 10 x 2500...

USART stops

Posted on April 01, 2018 at 15:36Hey guys,I am trying to receive the nmea sentences from my gps module. I am putting the received bytes in an array and if I get the '\n' I want to transmit the array. Problem is it only works once, then it stops:http...

Error: Flash Download failed - ''Cortex-M7''

Posted on April 01, 2018 at 12:58Hey guys,I used to be able to download my program to my stm32f723 discovery, but for some reason now when I want to flash even the untouched code, which I got by generating the stm32 cube project I always get errors:...

Noob question on ports

Posted on October 04, 2015 at 15:19 Hi all, Just plunging in again to learn STM32/ARM coding, and have a GPIO issue (on a STM32L100C discovery board): Why does this work... GPIOC->MODER |= (GPIO_MODER_MODER8_0 | GPIO_MODER_M...

arm_dude by Associate II
  • 1663 Views
  • 6 replies
  • 0 kudos

CAN Receive Error

Posted on March 30, 2018 at 10:25I'm working on STM32F412VET6 micro, & Configured CAN1 for communication & it is initialized as500Kbps, 75% Sample, ABP1 is @ 24MHzvoid CANInit(void){#ifdef LPBK_TEST CanTxMsg CanTxMsg; uint32_t uwCounter = 0; uint8_t...

0690X0000060AI0QAM.png

STM32L100-DISCO no COM port?

Posted on March 31, 2018 at 19:48Hi,I have an STM32L100-DISCO Board. I would like to askI have seen in the circuit diagram that the PA9 and PA10 Pins are connected to the USB to program the STM32L100 MCU. However, when I use the same PA9 and PA10 fo...