STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RDP Setting, HAL_FLASH_OB_Launch(), holding

Posted on April 09, 2018 at 04:17Hi.I am going to set the RDP-Level 1 programmatically.Here is the test code:Here it stops at the HAL_FLASH_OB_Launch () function.The Reset button does not work in this state.The USB connection will work only if you r...

stm32 2G module

Posted on April 08, 2018 at 04:03HI   I use stm32f107?now I want to communicate with a 2G gprs module by usb?How I do it ?#stm-32 #stm-32lo #stm-32f107 #stm-mcu

fan li by Associate
  • 1308 Views
  • 2 replies
  • 0 kudos

STM32f302cc SPI code assistance needed

Posted on March 25, 2018 at 22:51Hi,I have recently move from the STM32f101 to the stm32f302, I am using atollic IDE and the Hal library for the initial configuration of the peripherals.  I use register level setup for a lower overhead. having said ...

conrad c by Associate II
  • 3595 Views
  • 7 replies
  • 0 kudos

stm32R7VI widebus

Posted on March 24, 2018 at 10:29I met an interesting problem. When I tried to configure this IO with SD widebus config (4bit) with hal libraries I always failed with initialization because pin 1 of SD card is on logic 0.The solution was firstly let...

semler by Associate II
  • 2977 Views
  • 6 replies
  • 0 kudos

Resolved! Encoder mode and comparator?

Posted on April 08, 2018 at 09:59In the STM32F030x4/x6/x8/xC and STM32F070x6/xB reference manual (RM0360, ch 13.3.16) it says 'However, comparators are normally be used to convert the encoder�s differential outputs to digital signals. This greatly i...

STM32F411 Output pin connection while no VCC is applied

Posted on April 01, 2018 at 13:22Hello all,In my application, I'm controlling a secondary device using enable pin which has an internal pull-up resistor.The output pin is set to be ''0'' or open drain type output, and the STM32F411 VCC1 can be power...

0690X00000604X3QAI.jpg
Nir Alon by Associate II
  • 6980 Views
  • 17 replies
  • 0 kudos

Help to interface AT24C256 EEPROM with STM32F051r8

Posted on April 07, 2018 at 17:42I am trying to to write/read to at24c256.Iam new to I2C.I read about all theory stuffs.But i tried writing code from the i2c eeprom eg, but am not to able to skip the txis flag while loop.Please help.I commented the ...

Use of __libc_init_array call

Posted on April 07, 2018 at 18:36Hello,Into the startup assembly file there is a call to the __libc_init_array procedure, and i would like to know : What does it do ?If it is really essential ?What is the default implementation of the _init() proce...

oldone by Associate II
  • 1859 Views
  • 2 replies
  • 0 kudos

Resolved! Timer update DMA generation problem

Posted on April 07, 2018 at 16:30Hello! I'm working with stm32f042 MCU. My task is to read GPIO 8-bit data (7-0 bits) periodically, the faster, the better. I use timer 3 to generate DMA request and DMA channel 4. The idea is the following one: timer...

EvgenS Po by Associate II
  • 1908 Views
  • 5 replies
  • 0 kudos