Posted on December 13, 2017 at 11:50The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on December 14, 2017 at 15:09So you are suggesting to save/switch context inside high priority interrupt?Im a little bit confused becouse all ARM documents stands that PendSV should be used as context switcher in os enviroment.
Posted on December 14, 2017 at 09:40Inside the switch call, an interrupt with zero priority is called. So that it was impossible to interrupt the update procedure of the task stack.Where did you get it from ?freeRTOS is using only PendSV with priori...