STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB waveform abnormality

Posted on May 08, 2018 at 05:34Noise was applied to the board equipped with the STM32F302RC6, and the 0 potential level of USB_D + was raised. The applied point is not a USB terminal, and the USB cable is not connected yet. (The connection destinati...

INPUT CAPTURE for timer 3 and timer 13

Posted on May 07, 2018 at 20:54Hello, I have one input channel for timer. I notice PA6 either for TIM3-CH1 or TIM13-CH1. So it is possible to map pin for both of timers (3 and 13).  if I can do it, how to set them?Regards,

yang hong by Associate III
  • 1689 Views
  • 7 replies
  • 0 kudos

Resolved! ST Link does not work anymore!!!

Posted on May 07, 2018 at 20:19Hi.I was just programming my stm32f217 board via serial wire interface and everything was ok, but when I wanted to program once more the message ''No target connected''displayed and it didn't program my MCU anymore.But...

0690X00000604eFQAQ.jpg

HAL I2C DMA Detect NAK (STM32F072)

Posted on May 07, 2018 at 23:02I am using HAL I2C to interface Cryptomemory (from ATMEL). Using I2C master transmit(HAL_I2C_Master_Transmit_DMA), I need to differentiate the following two conditions of device,1. Send B4+ACK, 00+ACK, 00+ACK, 01+NAK2....

mtien888 by Associate II
  • 698 Views
  • 0 replies
  • 0 kudos

UART in STM32F407

Posted on May 02, 2018 at 17:24HelloI run into a stupid problem. I have a data that is sent by a device with bitrate115200. I need to read it with STM2F4. The data is five HEX numbers.I was trying to do this in different ways but I failed. I am read...

How DMA Transmit works ?

Posted on May 06, 2018 at 19:01Hallo everyone i have a question..as i know the DMA receives Data und when it reaches the Bytes the i have determined it makes interrupt so this is usefull because the cpu doesn't wait the UART slow connection to finis...

How should I set my ''heap'' and ''stack'' size

Posted on November 03, 2017 at 18:04After compiling the codes, my code size is:Program Size: Code=20140 RO-data=316 RW-data=540 ZI-data=2412 Based on this information, how should I set my 'heap' and 'stack' size? My first question is the 'heap' and ...

Vu.Andy by Associate III
  • 7429 Views
  • 7 replies
  • 0 kudos

ADC Vref?

Posted on May 05, 2018 at 11:02Hi,I beginner in stm32 i am using stm32l071 adc channel 9 what is vref ?vref is Vdda i am connect vdda as 2.5v this is internally connected to vref yes or not?can i enable vref by software(in code)?Sampling time variat...

Rewrite on a flash memory

Posted on May 07, 2018 at 14:33Hello, I am currently a French student placement and I program card NUCLEO-144 STM32F767ZI. I have some problems on the flash memory. I can write to the flash memory, read from the flash memory and erase a sector of th...