STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L100C-Disco board standby mode

Posted on May 02, 2018 at 23:01When using the STM32L100C-Disco Board i use the command,HAL_PWR_EnterSTANDBYMode()but when I measure the current on I_DDpins using a multimeter on the uA setting (using a Fluke 87), I read a value of ~282uA, which is h...

STM32F04 ADC multiple channel DMA single shot mode problem

Posted on May 10, 2018 at 08:02Hi ALL,I develop an application based on STM32F04. There are 3 ADC channels and I used DMA to collect data from these 3 channels.It can get correct data from ADC, but there is a problem.If I call the HAL_ADC_Start_DMA ...

jiangpen by Associate II
  • 684 Views
  • 0 replies
  • 0 kudos

STM32F4 CAN HAL

Posted on May 09, 2018 at 17:11Hello, For every peripheral like SPI,I2C,USART , etc, ST's HAL gives 3 types of apis like poll, IT and DMA . Why this is not applicable to CAN bus ? I dont find an api like can_transmit_IT or receive_it in the latest s...

n.serina by Associate III
  • 917 Views
  • 1 replies
  • 0 kudos

Reserve Flash for user data

Posted on May 09, 2018 at 12:28Hello,    I would like to save some data in the internal flash memory of an STM32L476. I found examples and guides and I was able to write and read data from flash. But I have a question: is the internal flash memory t...

STM32F407 PGPERR PGSERR

Posted on August 11, 2014 at 12:00 Hi, I'm having a peculiar issue when jumping from my application code back to my bootloader. Before jumping back to the bootloader I disable all peripheral as shown in the code below. But when the HAL_NVIC_...

joe by Associate III
  • 2337 Views
  • 5 replies
  • 0 kudos

Resolved! RS485 Driver Enable

Posted on May 08, 2018 at 19:44Is there somewhere a better description about this feature, than there is in the f070 reference manual? Maybe an example?I don't quite seem to understand how it's supposed to work. Or does CubeMX handle it somehow inco...

bor stm32 programming

Posted on May 09, 2018 at 18:12Can someone show me a simple program to read and write the option bytes on the STM32L476VGT using the STM32 HAL libraries? I only want to change USER parameters values, as the BOR level.I'm trying the following code, b...

Luis Ber by Associate II
  • 1101 Views
  • 0 replies
  • 0 kudos

GPIO pin behavior during JTAG programming

Posted on May 09, 2018 at 16:06Hi,this question may be hardware related. I saw some weird power ripple when I programming the STM32L4 device with JTAG. so can anyone explain what are GPIO status during JTAG programming? will it draw high current or ...

jeffz by Associate II
  • 894 Views
  • 1 replies
  • 0 kudos

STM32L4 Nucleo LSE drift

Posted on May 07, 2018 at 21:40Hi all,is there a way to improve LSE drift on L4 Nucleo board? Or all I can do is to migrate to another crystal with higher precision?Thanks, and regardsjerry