STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC1_IN16 (no mode)

I begin a new project I want to use the PA12 as a ADC input. But the pin is orange and I am unable to activate the mode or channel of the ADC.What is the explanation behind it? How do you explain it?Thanks a lot to all. 

carlesls2_0-1742466439720.png carlesls2_1-1742466529049.png
carlesls2 by Associate III
  • 1178 Views
  • 2 replies
  • 1 kudos

STM32L476 Changing VRef for ADC precision

Hi I want to sample low voltage signals with STM32L476 so I figured it would be a good option to reduce reference voltage and I found this part in the MCU datasheet: Now I am using ADC in dual mode and sampling 8 bit so it is not too precise for low ...

Stm325_0-1742410285083.png Stm325_1-1742410285211.png
Stm325 by Associate III
  • 1891 Views
  • 5 replies
  • 0 kudos

adding CMSIS-DSP library to stm32h743

hi,I want to use CMSIS-DSp library in my stm32h743 project. the project contain USb MSC device also.After adding the library to project i am getting 5 errors, which I am listing below,11:56:50 **** Build of configuration Debug for project DIN_MAIN_V3...

ykn by Senior
  • 1093 Views
  • 1 replies
  • 0 kudos

Resolved! Abnormal GPIO Operating Frequency on STM32H743IIT6

Dear Support Team,I am encountering an unexpected issue with my STM32H743IIT6 microcontroller where the GPIO operation frequency observed via an oscilloscope is only ​16.6 MHz, despite configuring the ​bus clock at 400 MHz and ​AHB clock at 200 MHz. ...

nhong by Associate
  • 1172 Views
  • 2 replies
  • 2 kudos

Resolved! QSPI external RAM

hi all,i was trying to work with stm32u585 microcontroller and an external RAM IS66WVQ2M4DALL , which is a QSPI based RAM can work in 133Mhz.the RAM support DDR based data transfer. Here i am attaching my OSPI configuration  hospi1.Instance = OCTOSP...

sabari1_0-1738740509990.png
sabari1 by Associate III
  • 4534 Views
  • 10 replies
  • 1 kudos

Resolved! How to update firmware over USB C

Hi,My board with a STM32F745VEH6 is working as a device, that need to be updated via USB C over time. How can I do that? Is there a way to update the firmware with command line?I tried to connect the micro over USB C with STM32CubeProgrammer, and got...

MF_GS_0-1742413158174.png
MF_GS by Associate
  • 2014 Views
  • 3 replies
  • 1 kudos

Resolved! STM32L476 Interleave and opamp

Hi, I am sampling high rate data using STM32L476 in Nucleo64 board in dual channel interleave mode. I am measuring very low voltage values so is it possible to use MCUs internal opamps together with interleave mode. It looks like I am not able to act...

Stm325 by Associate III
  • 1947 Views
  • 4 replies
  • 0 kudos