STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HardFault Handler while implementing I2C OLED.

Posted on June 18, 2018 at 09:59I am implementing a 3 channel frequency counter. So I get 3 different frequency values as inputs. I am using SSD1306 driver to interface the I2C-OLED. When I try to print only one of the frequencies, it works fine. Ho...

problème FOC librairie stm32f302R8

Posted on June 18, 2018 at 12:36Bonjour, Nous sommes entrain d'utiliser la stm32f302R8t6, la librairie FOC, un encodeur incrémental et la 3 shunt pour commander un moteur asynchrone (bldc). En effet, nous avons rencontré un problème avec la comma...

cubeMX 4.22 stm32f37xx lib 1.9 comp irq bug

Posted on September 10, 2017 at 05:06Hello! Code generated by CubeMX  v4.22 using  STM32F3 library v1.9 have the following bug:When enable comparator interrupt, C code generated in stm32f3xx_it.c use interrupt subroutine titled 'COMP_IRQHandler', wh...

xoserg70 by Associate
  • 3568 Views
  • 2 replies
  • 1 kudos

Can't Erase flash memory page

Posted on June 18, 2018 at 12:26Hello All.MCU: STM32F031G6U6IDE: System WorkbenchAPI: STM32F0 HAL and low-layer driversI am trying to erase page in the flash memory at address: 0x8002000.Here is the code:https://community.st.com/tags♯/?tags=code‌F...

FOC Lib Issue : Motor startup failure

Posted on June 18, 2018 at 11:53Hello,We are trying to command a BLDC motor using the FOC lib 4.3 and we notice the following behavior:- When the brake is activated (mechanical braking system) the motor is totally blocked and dose not start up even ...

stsafe_a100

Posted on June 16, 2018 at 18:54hello how i can get stsafe-a100 host library?thankshttp://www.st.com/content/st_com/en/products/secure-mcus/authentication-secure-iot/iot-secure-solutions/stsafe-a100.html 

End Node downlink problem

Posted on June 11, 2018 at 17:41Update:We solved our problem-Our gateway (improved single channel gateway based on WAZIUP project) sent with invertIQ=off for downlink and that caused the problem.Note: The answers given here were not correct, as LoRa...

Time based interrupt for lower values not working

Posted on June 18, 2018 at 09:03I exercised time based interrupt for 1 second on  stm32f0308(cortex M0) and for every one second I increment one counter variable .....this works fine ....I tested time based interrupt for 1 milliseconds too this also...

shital P by Associate
  • 1100 Views
  • 1 replies
  • 0 kudos

Problem with I2C-OLED interfacing

Posted on June 15, 2018 at 10:09I am trying to interface an I2C OLED display with an STM32L053C8 board. However, instead of using STM32CubeMX to initialize my different pins, I had to manually assign them, because the example programs which come alo...