STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem when programming for stm32f765

Posted on June 17, 2018 at 12:17Hi, has anyone worked with stm32f765 ? I'm now working with it in my project. I created my own PCB to test this stm32f7  , I have try  many time but anytime I test it, the stm32f7 always be damaged because I found tha...

SAI IO on pins from SAI example

Posted on June 16, 2018 at 05:58Hi,I am trying to change the SAI IO pins on the STM32F769_Discovery board using the SAI example.I would like to point the defined SAI block to arduino pins on the Discovery board so I can view them on the scope.I get ...

benyBoy by Associate II
  • 2758 Views
  • 5 replies
  • 0 kudos

Resolved! WHILE LOOP PROBLEM FOR MICRO SECONDS WITH TIMER ??

Posted on June 16, 2018 at 22:25Hi friends,The while loop does not work in the following function. Why could it be?For STM32F407VG;void US_BEKLE(uint16_t us){ uint16_t baslangic = (uint16_t)__HAL_TIM_GET_COUNTER(&htim1);while(((uint16_t)__HAL_TIM_GE...

BlueNRG-1 DIO11

Posted on June 17, 2018 at 12:34Hi,I used the BlueNrg-1 on a few projects but I have never had the problem before as I have never used DIO11. What concerns me that every is 100% when stepping through my code just before entering the BlueNRG_Sleep fu...

Use of clock dividers in timers (STM32F103)

Posted on October 25, 2014 at 16:02 Hi, I have just begun toying around with a STM32F103 (on a STM32 Nucleo board) and I have some troubles understanding the expected behavior of the clock divider in the timers. So my original goal...

alexpes59 by Associate II
  • 3567 Views
  • 3 replies
  • 0 kudos

STM32L072 Adc Vref source

Posted on June 16, 2018 at 20:16Hi,I'm a little bit confused about adc and vref.From reference manualThe internal voltage reference (VREFINT) provides a stable (bandgap) voltage output for theADC and Comparators. VREFINT is internally connected to t...

sukoy27k by Associate II
  • 2082 Views
  • 2 replies
  • 0 kudos

Working with TIM Output Compare

Posted on June 16, 2018 at 23:08I try to generate pulses for the stepping motor at the Output Compare output.The time between their leading fronts varies (acceleration / deceleration).The control of delays based on the well-known principle: free run...

0690X00000604hhQAA.jpg

STM32L4 QSPI flash memory mapped

Posted on June 16, 2018 at 14:32 Hello there, In the device I am developing on STM32L452 I foresee running out of flash memory, as the application code is getting bigger. The maximum flash amount for this chip is 512 KB (which I use). I thought I...