STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Incorrect low power current consumption CMWX1ZZABZ

Posted on June 21, 2018 at 16:03Hello,I design a LoRa aplication with CMWX1ZZABZ module. The schematic which I use is the following:And the current consumption es 1.2mA. Anybody know which are the errors in the schematic to get 1.65uA of the datashe...

0690X0000060LMZQA2.png

Resolved! DMA priorities for LTDC

Posted on June 22, 2018 at 08:57Hi,I have a problem with configuring priorities for DMA channels and LTDC controller.I am using a DMA channel to communicate with a DSP processor. In this channel I need a large data transfer. When I start the DMA cha...

Need I/O controller EVM board

Posted on June 05, 2018 at 06:30 Hi there, I have been back to high power design. My system contains 3phase, 380V, 50Hz ac input, secondary surge protector, Aux Tr ( single phase, 380V/220V, 300VA), phase transformer( 3ph, 380v/12v,0v,12v,100VA...

Resolved! CubeMX I2C Configuration issue with STM32H753IIKx

Posted on June 07, 2018 at 12:55Hello,I've created new STM32H753IIKx project with CubeMX(Ver4.26.0), and changed the I2C1/I2C2 setting into 'I2C' from 'Disable' in Pinout tab.And, switch to Configuration tab, open the I2C1 Configuration, move to GPI...

DMA_DeInit implementation CCR overwrite?

Posted on June 20, 2018 at 18:27In the stem32f10x_dma.c the DMA_DeInit function has the following lines: /* Disable the selected DMAy Channelx */ DMAy_Channelx->CCR &= (uint16_t)(~DMA_CCR1_EN); /* Reset DMAy Channelx control register */ DMAy_Channe...

STM32F042 Is HAL_CAN_ConfigFilter() required?

Posted on June 18, 2018 at 23:06 I'm trying to get an interrupt-driven CAN receiver working on a STM32F042K6- but I'm not having much luck. I'veconfigured the CAN module in CubeMX and the code it generates makes sense to me - and seems to match t...

STM32F3 Interrupt and timers

Posted on June 21, 2018 at 10:56I am running STM32F303VC.I require an IRQ on GPIOE_Pin_15  ---> TIM2_Channel_1My typical Frequency range is from 5 Hz - 500HzThis is required to provide me with a number of ticks between the 2 interrupts.  The result ...

kim by Associate
  • 2895 Views
  • 3 replies
  • 0 kudos

STM32L496ZG flash program issue

Posted on June 21, 2018 at 00:57Hi,I am working on STM32 flash program using a sample program from V1.11. The program is pretty straight forward. Erase ADDR_FLASH_PAGE_16 to ADDR_FLASH_PAGE_255 then program.The program stuck in HardFault_Handler doi...

LL_GPIO_Init on STM32F103

Posted on June 20, 2018 at 23:24I am trying to initialize GPIO ports on STM32F103C8 using the LL library. When I set up pin PC13 by a sequence of individual calls (LL_GPIO_SetPinMode, LL_GPIO_SetPinOutputType), it is initialized correctly. However, ...