STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem in MSC_Standalone

Posted on June 27, 2018 at 07:05I use mass storage sample from STM32Cube_FW_F4_V1.21.0\Projects\STM324xG_EVAL\Applications\USB_Device\MSC_Standalone on STM32F40G-EVAL When I format a partition with a NTFS and exFAT system file and copy a large file(...

mostafa z by Associate II
  • 1028 Views
  • 1 replies
  • 0 kudos

Problem in MSC_Standalone example

Posted on May 17, 2018 at 12:13HiI use mass storage sample from STM32Cube_FW_F4_V1.21.0\Projects\STM324xG_EVAL\Applications\USB_Device\MSC_StandaloneWhat kind of file systems does this example work?Does it work with the NTFS file system?

mostafa z by Associate II
  • 2658 Views
  • 6 replies
  • 0 kudos

Using USB-OTG in MSC_HOST mode

Posted on June 28, 2018 at 09:47Hello! I started working withhttp://mikrocontroller.bplaced.net/wordpress/?page_id=383. Apparently there are errors in it, since I can not connect to USB-Flash yet. I adapted this project STM32F105RCT6 microcontroller...

Failsafe upgrades with STM32L476 Dfu

Posted on June 27, 2018 at 15:24On the STM32L476, we have been using the Dfu program that comes loaded in system memory.We've been using this ROM code succesfully as a way to load firmware on to the MCU flash over USB, with the documented Dfu file f...

Why does STM32Cube recommend to not use SysTick

Posted on June 27, 2018 at 22:08as TimeBase Source?Today, I've been trying to activate FreeRTOS' USE_TICKLESS_IDLE feature.It turns out that the tickless idle --in fact it is a unnecessary tick suppression-- works only when Timebase Source is SysTic...

cube_mx 4.26.0+STM32Cube FW_F4 V1.21.0ç�?Ÿæˆ�的代ç �编译ä¸�通过

Posted on June 28, 2018 at 05:54cube_mx 4.26.0+STM32Cube FW_F4 V1.21.0,一但使能了sd�?�+fatfs+freertos�?�,生�?的代�?就编译失败。麻烦修正一下,谢谢。编译报错:这里�?�有两个问题:1.main.h循环包�?�。�?�: main.h-->#include ''stm32f4xx_hal.h'' --> #include ''stm32f4xx_hal_conf.h''-->#include ''m...

0690X0000060LUsQAM.png

Resolved! STM32F4cube examples - but where ?

Posted on June 27, 2018 at 16:17Dear Community,I’ve just installed the STM32F4cube from SetupSTM32CubeMX-4.26.0.exe  but I cannot find the “Hundreds of examples for easy understandingâ€� mentioned on https://www.st.com/en/embedded-software/stm32...

M G_2 by Associate III
  • 1863 Views
  • 2 replies
  • 0 kudos

STM32F765 to eMMC integration issues

Posted on May 17, 2018 at 10:04 Dear All We are facing some issues on eMMC integration with STM32F765 micro controller , In STM32CUBE we generated SDIO interface source code , eMMC manufacture is says this source code was SDcard interface. How we...

nagaraj by Associate II
  • 6747 Views
  • 14 replies
  • 0 kudos