STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 with nRF52

Posted on July 01, 2018 at 15:03Hello all.I would like to use the nRF52 for supporting Bluetooth 5. I see the previews example connect STM32L4 to nRF51 using the UART support by the CUBE. I don't find a dedicate examples in ST or a developer tools t...

Barbie by Associate II
  • 1794 Views
  • 1 replies
  • 0 kudos

Use CUBEMX FREERTOS HAL_TIM,go to hardfault

Posted on June 30, 2018 at 16:38 I use the cubemx and freertos andSTM32Cube_FW_L1_V1.8.1,use the timer2 as the systick,but run theosKernelStart() function, a hardfault occurrence. use the timer3 as the systick,it`s OK.ThenChange back to timer2,it...

0690X0000060By6QAE.png
cs c by Associate II
  • 2120 Views
  • 4 replies
  • 0 kudos

CAN Timed Transmission

Posted on June 30, 2018 at 11:44Hello, The RM says that CAN1 has 16 bit free running timer, can we use this to Tx CAN message at desired interval ? if possible ,  how to set the desired time period ? or should is use any timer peripheral for my use ...

RN by Senior
  • 842 Views
  • 1 replies
  • 0 kudos

STM32 Stpper Motor (PWM +DMA)

Posted on January 20, 2014 at 16:12 Hieverybody, I have aquestion regarding a stepper controller firmware provided by ST. Actually I do not get the DMA run on my STM32F107! The capturecontrol toggle mode is working, but no other values are ...

LPTIMER ARR INTERRUPT?

Posted on June 29, 2018 at 10:09Hi,I have configured ARR register to 0x0000000A and Enable ARR interrupt  interrupt not generate after 0x0000000Abut after 1 extra one pulse generate interrupt

USB_OTG FS mode doesn't work on discoveryf746

Posted on June 30, 2018 at 08:27Hello.We have a project on discovery f746 board that we've run RTOS and emwin on it.Now we want to add USB_OTG FS mode for sending data on Flash memory in MSC mode.For this purpose we attached configurations file of M...

What is the use of PDR ON ?

Posted on June 28, 2018 at 22:53hello .1.We have  done a Stm32F429 board , and we can set PDR ON to GND OR VCC (we set to gnd)how ever in the  STM32 PDF : AN4488 Application note  STM32F4xxxx MCU hardwareit says in  IN    ....3.2.1 PDR_ONPDR_ON = 0 ...

maor by Associate III
  • 9765 Views
  • 3 replies
  • 1 kudos