STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Wrong value of VCAP capacitors in STM32F407VGT board

I have 10uF (=10uF+100nF)ceramic capacitors for VCAPs in a custom board. Voltage there is 2.7V. Supply voltage is 3.3VI have problems getting the STlink to accept the board. First I managed to erase the chip, now STLink does not even recognise the c...

LMI2 by Lead
  • 4313 Views
  • 10 replies
  • 0 kudos

Is Full Duplex Possible with DMA and how to use it with CubeMX

Hello there,up to now i have used an Audio DAC on a STM32F407 with DMA and Half/Full Transfer Interrupts with CubeMX. So far so good.But now i am a little bit confused. As i have read some Posts it seems that it might be not possible to use Full Dupl...

RBoel by Associate
  • 1896 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F7X internal regulator won't start

hello I am using the STM32F779NXH MCU it has an internal 1.2V voltage regulator that I believe should output volt on the CAP_1 and CAP_2 pins. The MCU will not boot, and will not be recognized by the st-link. This is a brand new board and has never ...

TallGUY by Associate II
  • 2129 Views
  • 2 replies
  • 0 kudos

ST-LINK Issue - Target unknown error 5010512

Hi,I am seeing the issue since yesterday for unable connect to target. Here is the message from TrueSTUDIO. Unable to connect using STM32 ST-LINK Utility as well.I am guessing the ST-LINK device burned. We are using tag-connect TC2050 adapter and con...