STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to find a Temperature on STM32F303K8

Hi, Everyone.I'm tring to make adc sensor works, to find a temperature.I found AVG_Slope and V_25 in the datasheet: AVG_Slope = 0.0046 V_25 = 1.46And I used V_Ref = 3.0f and N_Bit = 4096fThis is My code (Only for adc_complete conversion)void HAL_ADC_...

How to use SPI3 of STM32F103RCT6 (no have SCK)

Dear AllNice to meet you. At First My english is poor. Please understand me.I want use M95512 (EEPROM) with STM32F103RCT6 SPI3but now I check Oscilloscope SCK, MOSI, MISO. Only work MOSI have signalnow no work SCK.... How to Init. SPI3 Please check m...

NAND memory readback error

Hello,I'm using a NUCLEO-L496ZG-P board together with a Samsung K9F1G08U0E nand module. At the moment i'm testing read write operations. For certain values what i read from page differs from what i've written. For instance if i fill page with rand() ...

Resolved! STM32L4R9 strange behavior when awaking from shutdownMode

Hello,I enter the shutdown mode with the following code statementHAL_PWR_EnableWakeUpPin( PWR_WAKEUP_PIN1_LOW ); HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN2 ); HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN3 ); HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN4 ); HA...

s m by Associate III
  • 1083 Views
  • 1 replies
  • 0 kudos

Nucleo-H743ZI No data out in I2S slave mode

HI, I'm trying to interface this board to a cirrus logic CS42448 codec. I set up the I2S3 peripheral in slave mode configured in CubeMX as so:The project is built with this and in the main while loop I have a simple bit of code to get it to transmit ...

0690X000006BzZyQAK.png
savvn001 by Associate II
  • 1954 Views
  • 4 replies
  • 0 kudos

NRST Reset functionality on the STM32F205VCT

Hi,I wish to hold the STM32F205VCT in reset for X time whilst other hardware is initialised.I have a hardware timer circuit linked to the NRST pin.As this is a safety related system, I am trying to establish the NRST / reset functionality...The reset...

RYoun by Associate
  • 1343 Views
  • 2 replies
  • 0 kudos

Bug in IRQ management during HAL Library initialization

STM32CubeMX version : 4.26.1Chipset : STM32F207VCTHello,In HAL code initialization, the code don't manage correctly the Interrupts initialization. I found this bug in UART part, TIM2 (use for FreeRtos) part and ETH part.Every time the software launch...

Teseo II STA8088 X-loader timed out error

Posted on September 01, 2017 at 11:03Hi, I've been trying to perform a FW update on a Teseo II GPS module using the X-loader. However, after the 'Sending the bootloader through UART......' message, the X-loader always returns with a 'timed out' erro...

CMSIS_OS.h warning - osThreadDef, warning: initialization from incompatible pointer type [-Wincompatible-pointer-types]

Posted on May 01, 2018 at 03:41Has anyone seen this warning while using FreeRTOS?  The full define is :#define osThreadDef(name, thread, priority, instances, stacksz)  \const osThreadDef_t os_thread_def_##name = \{ #name, (thread), (priority), (inst...