STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PWM and ARPE

I was trying to figure out what datasheet says with the following sentence highlighted bold for STM32F303R8T6The PWM mode can be selected independently on each channel (one PWM per OCx output) by writing ‘0110’ (PWM mode 1) or ‘0111’ (PWM mode 2) in ...

BG1 by Senior
  • 1807 Views
  • 2 replies
  • 0 kudos

Tick timer problem in STM32CubeExpansion_LRWAN_V1.2.0 firmware.

Hello!I have problem with Tick functions in this firmware."HAL_GetTick()" function always returns value 0.Also some functions that use timeout doesn't exit on timeout situation because they count on "HAL_GetTick()".Could somebody help me to start Tic...

LMehm by Associate III
  • 574 Views
  • 0 replies
  • 0 kudos

STM32F103XB: TIM2 CH1 on PA15 conflicts with SPI1 NSS

Posted on January 09, 2018 at 18:32Hi,Using CubeMX, I configured SPI1 on a STM32F103T8Ux as full-duplex master mapped on PB3..PB5, with hardware NSS (on PA15) disabled (set to SPI_NSS_SOFT in spi.c).So, PA15 should be available for TIM2 CH1 PWM outp...

Problems: STM32H743ZI two SPIs to receive data with DMA

Hello,I use STM32H743ZI two SPIs with DMA to collect data. The data are OK when only one SPI with DMA is activated. However, when I use two SPIs with DMA to collect data simultaneously, the data collected are not correct. The DMA setup:Codes to colle...

0690X000006C7kIQAS.png 0690X000006C7kNQAS.png 0690X000006C7kSQAS.png 0690X000006C7kXQAS.png
MSun.5 by Associate II
  • 2093 Views
  • 4 replies
  • 0 kudos

STM32F746G-DISCO - demo displays :scrambled'' pictures

Posted on September 04, 2017 at 21:53Hi,I had a few STM32F746-DISCO boards. This time I bought second hand board and uploaded demo app.All pictures are 'scrambled'. I cannot figure out what is going on. Seems like a hardware defect.Please share your...

Non linearity in ADC Measurement using STM32F051R4T6TR IC

Hai,i have been into designing a solar inverter using STMF051R4 series IC for past few years. Presently we are working on ADC Measurement with DC voltage.The problem we are facing now is we not able to get a linearity in measurement of the dc voltage...

Amal Babu by Associate III
  • 12565 Views
  • 28 replies
  • 0 kudos