STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB charging with data transfer

I want to charge the Android phone along with USB data transfer. I am using STM32F072C8T6 as micro-controller and NCP1855 for mobile charging.The problem is this, in some mobile phones the charging is happening but the USB is not getting detected(And...

ayedu by Associate
  • 985 Views
  • 1 replies
  • 0 kudos

How to load an user defined external loader in ST-Link

I have created an external loader for S29GL032 NOR FLASH using STM32F051 as target.The code in "loader_SRC" is rewritten from M29W128GL_STM3210E-EVAL project for TrueStudio using GPIO direct insted of FSMC.The problem is that I can't see the loader ...

pese by Associate
  • 851 Views
  • 1 replies
  • 0 kudos

i2c function of STM32F051R4T6TR

Hai,i am using STM32F051R4T6TR in my design.When i checked my datasheet i could just find the additional functions of the port A and Port B in the datasheet.But couldn't find details regarding additional functions of the PORT C and PORT F.Even though...

Amal Babu by Associate III
  • 679 Views
  • 0 replies
  • 0 kudos

Understanding STM32 Sub-families

I have selected the STM32F091RCT for a new design and was having trouble understanding a specific section of the naming schema -Example: STM32F091RCTSub-family: '91'0: Value line1: Access line2: USB line8: Low-voltage lineThe '1' makes sense this is ...

Justin1 by Senior
  • 1801 Views
  • 2 replies
  • 0 kudos

STM32L452RE Nucleo Board

​Based on STM32L452RE specification, it can support from 1.71V to 3.6V. I have try using external 3.3V power supply to power up the board. Q1, However when I change the voltage from 3.3V down to 1.8V, the reset signal voltage level change. At this po...

ychua by Associate
  • 702 Views
  • 2 replies
  • 0 kudos

Ethernet IAP doesnt work with newer browsers. How to fix?

Hello, I got the IAP example running and found that it does not work properly with newer browsers (i tried Chrome, Firefox, Edge, all of newest version). The index page loads fine, but when the user and password is posted, the upload page does not lo...

Thomas K by Associate II
  • 1931 Views
  • 5 replies
  • 0 kudos